Configuration

Before you begin

To operate the device in a cybersecure environment, take the following measures before commissioning:

  • Change default user and add a strong password. Secure the password in a safe location.

  • Check if the device is running the latest firmware version. If not, update the firmware to the latest version that fits your needs.

General settings

Fieldbus integration

The following configuration guides are available for the supported fieldbus protocols:

IIoT integration

The following configuration guides are available for the supported IIoT protocols:

Terminology, acronyms

Post-commissioning measures

In order to maintain a secure environment, take the following measures after commissioning:

  • Create a backup of the device configuration and store it in a secure location.