WebUI/web interface

General

The network module includes an integrated web interface for accessing detailed device information and for configuration.

Prerequisites

To use this web interface, it must be ensured that the module has been integrated in the network correctly. To do this, the IP subnet of the network module must be accessible from the PC on which the browser is being operated.

Browser

The web interface is compatible with newer versions of Google Chrome, Firefox or MS Edge.

Note

For more detailed version information, see the data sheet at www.balluff.com on the product page.

Connection setup

  • To establish a connection with the web interface, enter the IP address of the BNI module in the browser’s address bar.
    ⇒ WebUI starts with the homepage, which displays the most important device information (see Homepage).

In the top window area, there is a navigation bar which enables you to switch between the different dialogs of the web interface by clicking on the corresponding icons:

../../../_images/navbar.png

Navigation bar

Note

Hover the mouse over the different icons to see the corresponding names.

User profile

Click on the user icon

../../../_images/BET_Menu_Benutzer-Icon_neutral.png

to open a user menu:

../../../_images/Benutzermenue_nicht_angemeldet_EN.png

User menu (not logged in)

When logged in, users with the ADMIN role can also see the user management (see User menu (logged in)).

Users with the EXPERT or USER role will see the entry Edit profile here instead, through which the respective profile can be viewed and, if relevant, edited.

../../../_images/Benutzermenue_angemeldet_EN.jpg

User menu (logged in)

Information/documents

Click on Help > About to view device-specific information and documents.

../../../_images/Benutzermenue_Hilfe_EN.png

User menu: Help > About

Use the dropdown menu under Online documents to select different online documents, such as manuals, and click on them to open in a new window.

Language selection

The languages German and English are supported. Click on the language German or English to select the language.

../../../_images/Benutzermenue_Sprachauswahl_EN.png

User menu: Language selection

User Management (ADMIN)

Select User Management to open a view of the stored users. Information on the user status (active/inactive), the user name, user information, password and its confirmation in hidden view, as well as the user’s role is specified.

../../../_images/Benutzerverwaltung_EN.png

User Management

Authorizations are role-dependent:

User rights

Authorization

ADMIN

EXPERT

USER

Read device parameters

X

X

X

Write device parameters

X

X

–

Adding users

X

–

–

Deleting users

X

–

–

Click on the pen icon to edit fields and buttons.

../../../_images/DE_7.1.3_loeschen_button.png

Pen icon

Click on the information icon in the password field to open a dialog box and view the requirements for a secure password.

../../../_images/Informations-Icon_im_Passwortfeld_DE.png

A user with the ADMIN role can delete users with the EXPERT or USER role by clicking on the recycle bin icon.

Note

The default user admin can only be deleted if another user with admin rights exists.

Click on + (Add new user) to add new users and confirm with

../../../_images/DE_7.1.2_speichern_abbrechen.png

after entering the corresponding information.

Edit profile (EXPERT/USER)

Users with the EXPERT or USER role can view and, if relevant, change their profile via Edit profile. Only the relevant profile is displayed. EXPERTs and USERs can only change their own user information as well as their own password, but not their role or name. EXPERTs and USERs cannot make any profile deletions.

Logging in and logging out

Note

Several PCs can access the network module with read access at the same time (without login). However, parallel accesses can result in response delays.

To make configuration settings on the network module via the web interface, you must first log in with the EXPERT or ADMIN role. Logging in with the USER role activates further dialogs in view-only mode. The user icon indicates the current status.

User icon

Not logged in

Logged in

Login

  1. Login (see User menu (not logged in)) opens the login dialog.

    ../../../_images/Anmeldedialog_EN.png

    Login dialog

  2. Enter the login details and click on LOGIN.

Note

Logging in is required when notifications request it or when selecting functionalities that cannot be used without logging in.

Each device has its own default password for the admin user. It is printed on the side of the device and is only used for the first login, or it is required when the network module is reset to factory settings.

As soon as the password for the admin user is changed, it is no longer possible to log in with the printed default password.

../../../_images/P067_Seitenansicht_Bild_Neu_3-12.png

Default password on the side of the device (example)

Note

On a new device it is possible to log on within 60 minutes after the device starts with the admin user and a random or blank password if no login has already been carried out on the new device.

Log out

  • Log out with Logout (see User menu: Language selection).

    Note

    If there is no interaction with the WebUI for more than five minutes, the user will be logged out automatically.

Homepage

The homepage shows information about the network module itself and its network activity. It also shows whether the configuration lock has been activated via the control unit (PLC).

../../../_images/WebUI_Startseite_EN.png

WebUI – Homepage

Port overview/configuration

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

If an IO-Link device is connected to one of the configured IO-Link ports, the module data at the ports and the device data are displayed in buttons on the left-hand side of the figure. After one of these buttons is selected, the corresponding port dialog opens. The default value of the displayed DeviceAlias is adapted to the labeling on the front.
The port numbering always starts at 1, even if the labeling on the front has a different port designation depending on the product variant. This is due to the relevant definition of port numbering in the IO-Link specification and the IO-Link/JSON specification (JSON Integration for IO-Link, Karlsruhe, 2020). The designation of the front label is reflected in the process data layout as well as in the description file (GSD).

Device Status

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

Some devices (including from external providers) supply the device status defined in the IO-Link Spec. In this case, it is displayed on the home screen. On the homepage, details can be called up by clicking on the icon in the port (see Fig. 8-13). Products that do not supply the device status show a gray control box here.

../../../_images/Device-Status_EN.png

Device Status

Opening the port dialog

  • Click on the corresponding port field to select the desired IO-Link Port.

    ../../../_images/IO-Link-Port_Breadcrumb_waehlen_DE.png

    Selecting the IO-Link port in the breadcrumb

  • Alternatively, select the target port via the breadcrumb navigation in the header.

    ../../../_images/IO-Link-Port_Breadcrumb-Navigation_EN.png

    Selecting the IO-Link port in the breadcrumb navigation

Note

The IO-Link device data is only displayed if the port is configured as an IO-Link port (can be identified by the green port LED).

Ports dialog

../../../_images/Portdialog_EN.png

Ports dialog

Click on the expand symbol of a closed tab page to view e.g. information on relevant ISDU parameters. Information that is not currently required can be hidden by clicking on the collapse symbol .

General Information

Under General Information, you can find manufacturer information as well as other general information on the current module. Under IODD, you can see whether a suitable IODD for the IO-Link device connected to this port is uploaded to the network module.

../../../_images/IODD_DE.png

IODD

If this is not the case, click on Upload IODD to access the Settings tab page. Based on the connected IO-Link devices, the corresponding device description can be selected for upload.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

Process data

Under Process Data, interpreted data is only shown if a suitable IODD is saved. To display the data more clearly, information from the device’s IODD is used here. So, in IODD Interpretation, you can see not only the input data of the example sensor as a hexadecimal number, but also interpreted under Input and provided with corresponding labels from the IODD.

In the Set process data area, the output process data of an IO-Link device can be set manually. The Validity Qualifier can be used to specify whether the process data should be marked as valid or invalid (PD valid).

../../../_images/IODD-Interpretation_EN.png

IODD Interpretation

Parameter (IODD)

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

Note

The Parameter (ISDU) tab page is only displayed if a suitable IODD is uploaded for the IO-Link device connected to the selected port. Upload IODD , see General Information.

Under Parameter (IODD), the device identification data of the IO-Link device is displayed in a table when the Identification tab page is selected (e.g. Dialog view after clicking on Read all or, for each subindex, on Read). The corresponding texts are saved in the IODD.

The input values can either be read out from the IO-Link device individually for a subindex by clicking on Read or for the entire tab page via Read all. A successful request is indicated by a green bar on the right-hand edge of the relevant table row.

../../../_images/Dialogansicht_EN.png

Dialog view after clicking on Read all or, for each subindex, on Read

The Application Specific Tag is an application-specific field in IO-Link devices and, in the current example (see Application Specific Tag), can either be read out from the IO-Link device with Read or can be individually configured by clicking on the gray input field with the same name and described with Write (provided the required write authorization exists). It is also possible to enter a company-internal device name in this field.

../../../_images/Application_Specific_Tag_EN.png

Application Specific Tag

If the IODD of the IO-Link device at the currently selected port also has parameters, these are also displayed in the form of a table (see Ports dialog figure). Similarly to the process for device identification data, parameter values and associated texts from the saved IODD can be configured, depending on the parameter, via Read or Read all.

If available, click on the ▼ icon to open a dropdown list and select a value or select a value within a specific range and confirm with Write.

If there is no Read button next to subindices, these indices cannot be processed individually, but only as a complete index.

../../../_images/Dialog_Ports_EN.png

Ports dialog: Extract from the parameter list of an IO-Link device with uploaded IODD after clicking on Read all or Read for individual subindices

Note

Each changed value must be written individually by clicking on Write !

ISDU Parameter

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

Configuration parameters of the IO-Link device can be read and written via the ISDU Parameter option. The parameter indices and subindices of the IO-Link device follow the IO-Link conventions and are described in the corresponding user’s guide.

Parameter indices and subindices can be entered both in decimal and hexadecimal format, while data can only be entered in hexadecimal format.

An input is confirmed with Set or can be rejected with Delete.

Events

Under Events, you can see whether there is a diagnosis event from the IO-Link device.

The events can be displayed in ascending or descending order. The list of events can be updated via further options of the Events card or can be downloaded in CSV format.

../../../_images/Weitere_Optionen_Events-Karte_EN.png

Further options of the Events tab page

LEDs

The LEDs of the network module display information on the current process data and the module status. The meanings of the LEDs can be viewed in a legend.

Opening the LED legend

  • At the LED legend, click on OPEN.

    ../../../_images/LED-Legende_aufrufen_EN.png

    Opening the LED legend

    ⇒ The legend appears.

    ../../../_images/LED-Legende_EN.png

    LED legend

Condition Monitoring

Note

This function is only available for XG5 devices.

../../../_images/Condition_Monitoring_EN.jpg

Condition Monitoring

Click on the corresponding icon in the navigation bar (see Navigation bar) to open the Condition Monitoring dialog.

Module values

In the top section, you can see the condition monitoring values of the module that are not port-specific. These values relate to the entire module and are refreshed automatically every 10 seconds.

Electrical values

The table on the Electrical Values tab shows the available values for current consumption and power draw at the individual pins of the different ports.

../../../_images/Elektrische_Werte_EN.png

Electrical Values

Diagnosis

Click on the corresponding icon in the navigation bar (see Navigation bar) to open the Diagnosis dialog. The Diagnosis dialog provides general service information about the device and a logging function.

The Status tab page contains information for all service requests, while the Activity Log tab page contains a table view of the log information. The information can be printed as a PDF by clicking on the printer icon (e.g. for a service request).

Note

If you have a specific question about a specific case, save or print this website as a PDF file and send it to us for technical support. You can find the corresponding contact details at www.balluff.com.

Information

Via the Information item, you can view information about the device, such as the browser version used or the system operating time.

../../../_images/Informationen_EN.png

Information

Activity log

The Activity log displays events in their chronological order and is an important tool for detailed troubleshooting in plants.

The expanded Activity Log tab page provides a table view of the log information, which can be sorted by number. The log information consists of a severity indicator, a date stamp, information on the origin, and the log message itself.

../../../_images/Aktivitaetsprotokoll_EN.png

Activity log

Events are classified via the Severity column:

  • Internal error (Emergency, Alert, Critical)

    The network module has detected an internal defect (hardware or software) that should not normally occur. If this happens, the module must be serviced or replaced.

  • External error (Error, Warning)

    The network module has detected a potentially impermissible event that is affecting the module from an external source. Troubleshooting within the system may be necessary.

  • Event (Informational, Notice)

    The network module has detected a significant normal operating event (such as configuration actions via the web interface and other configuration interfaces, which are recorded) and reports it.

Under additional options ( ), you can access further actions for the log (the log entries are stored in a ring buffer):

  • Refresh

  • Download CSV

  • Clear

Settings

The Settings dialog enables the configuration of connected modules and IO-Link devices. Click on the corresponding icon in the navigation bar (see Navigation bar) to open the Settings dialog.

Note

Changing and saving settings as well as implementing restarts and resetting to factory defaults can only be performed by users with corresponding authorizations (ADMIN , EXPERT ).

General settings

General settings such as the name of the module, the module time and security configurations can be made under General.

../../../_images/Modulzeit_einstellen_EN.png

General tab

Settings can be applied by clicking on SAVE and permanently stored in the device.

RESTART restarts the module (like switching the power supply off and on).

RESET TO FACTORY SETTING completely deletes the configuration saved in the device and then performs a reboot. The device is reset to the delivery state.

Manually setting the module time

  1. Under General > Module time, either click on the calendar icon or use the Set from PC dialog to transfer the current browser time to the network module.

  2. Apply the settings with SAVE.

    Note

    The module time is not permanently stored. After a reset, reboot or power, the time will be reset to the factory setting.

Retrieve module time automatically

An NTP server can be configured from which the time is automatically retrieved.

  • Under General > Module time, select the option NTP server activated.

  • Under Synchronization interval, select how often the time is retrieved from the NTP server.

  • Enter the IP address of the NTP server under NTP server address (internal URLs are not supported).

  • Apply the settings with SAVE.

Making security configurations

The following security settings for the REST API interface can be made using the security configurations.

Soft Session Timeout

Defines the time in seconds after which a user is logged out in the event of inactivity.

Hard Session Timeout

Defines the time in seconds after which a user is logged out, even if they are active.

Minimum Password Length

Defines the minimum required password length for newly created users.

Rest API Security

Activates or deactivates authentication when using the REST API directly. If deactivated, it is no longer necessary to log in and send the session token and cookies with a request. All requests have the rights of the ADMIN user.

Make network settings

Under Network, the IP Address, Subnet Mask and Gateway Address fields can be reset separately via the FACTORY DEFAULT button (see Security Management).

The Storage setting can be used to select how long the new network configuration should be valid.

Permanent

Saves the settings after a restart.

Temporary

Saves the settings until the next restart (factory setting).

The factory settings then apply.

../../../_images/Netzwerkeinstellungen_EN.png

Network settings

Security Management

Security Management can be used to enable or disable unencrypted and encrypted communication with the web server using HTTP(S).

../../../_images/webui_securitymanagement_en.png

security management

Note

If the connection between the web browser and the BNI is made via a HTTPS connection, the BNI provides a self-signed certificate that must be imported into the web browser. When the connection is opened, a warning appears in the web browser which must be accepted. After accepting, the certificate is imported.

If the IP address changes, the old certificate may have to be deleted and the new one imported. Once the certificate has been imported, the WebUI opens. A warning symbol appears in the URL bar, but this can be ignored.

Change protocol

The active fieldbus protocol can be viewed and changed in the section Fieldbus Protocol.

../../../_images/Protokoll_aendern_EN.png

Change protocol

I/O ports

Via the I/O Ports dialog, the ports of a module can be displayed and configured.

Select Set configuration for all ports to set the IO-Link [Autostart], Digital In and Digital Out configuration modes to the desired mode for all ports.

../../../_images/Einstellungen_IO-Ports_EN.png

IO Ports settings

Click on SET ALL to open a dialog window in which the action can be confirmed or canceled. With a corresponding selection, the message I/O port configuration(s) successfully saved appears in the bottom part of the website.

../../../_images/Alle-Setzen-Dialog_EN.jpg

Set All dialog

The ports can also be configured individually. The inputs are confirmed with SAVE or reset with UNDO.

The following parameters can be configured (see IoT/IIoT):

Device Alias

name of the device that shows what function the sensor executes (e.g. rear left end switch, temperature at boiler floor, etc.)

Modus Pin 4

selection of the actuation (e.g. Deactivated, IO-Link [Manual], IO-Link [Autostart], Digital in or Digital out. Depending on the selection, further dialog fields open, which require an input (e.g. when the IO-Link [Manual] option is selected).

Validation and Backup

Settings see Validation & Backup.

Cycle Time

if the IO-Link [Manual] or IO-Link [Autostart] options are selected for point Modus Pin 4, the desired communication cycle can be set by selecting the corresponding value from the dropdown list.

Modus Pin 2 (CLASS_A)

selection of the options Digital in or Digital out.

Current pin 2

Maximum current at which the pin switches off. Can only be configured if the pin is configured as an output.

Current pin 4

Maximum current at which the pin switches off. Can only be configured if the pin is configured as an output.

../../../_images/Dialog_Auswahloptionen_EN.png

Modus Pin 4 selection options dialog and Port 2: Configuration dialog of the IO-Link [Manual] option

Note

Automatic Shutdown of Pin 1 Power on Port Deactivation:

If a port is configured to deactivate Pin 2 and Pin 4, the power supply on Pin 1 is automatically shut down.

UA Configurable behavior

The behavior allows the IO-Link master outputs to be influenced in the event of a sudden loss of actuator voltage UA.

../../../_images/UA_configurable_WEBUI.png

UA Configurable behavior

There are two selection options:

US outputs shut down on UA powerloss
All active outputs on Pin 2 and Pin 4 are automatically switched off in the event of a UA voltage drop.

Hardware defined
Only all active Pin 2 outputs of the Class B ports are switched off in the event of a UA voltage drop. All other outputs remain in their current state.

Note

Only available for the XG5-538-…-variants.

IoT/IIoT

The IoT settings of the device can be made via the IoT dialog.

  • MQTT

  • REST API

  • OPC UA

In this manual, the acronyms IIoT (Industrial Internet of Things) and IoT (Internet of Things) used.

MQTT client settings

The BNI features an MQTT interface that allows parameters and product information to be called up. The BNI acts as an MQTT client whose messages are sent cyclically. For events, the BNI sends messages to an MQTT broker (PUBLISH). Other MQTT clients, e.g. applications that store data in an external database, can subscribe to topics provided via the MQTT broker (SUBSCRIBE).

The data sent via MQTT can be used, for example:

  • for Condition Monitoring

  • as an interface to Track&Trace applications

  • for further processing in the cloud

../../../_images/MQTT-Client-Einstellungen_EN.png

MQTT client settings

Connection status

The following information can be viewed:

  • Status: Indicates whether the client is connected or there is an error.

  • Address: Displays the address of the broker to which the client is currently connected.

  • Uptime: Displays the elapsed time in seconds since the connection was established.

IODD status messages

Indicates whether the correct IODD could be found and loaded for each device and which value is used for any condition variable. The correct IODD is required to send parsed IO-Link data.

In addition, the IODD can be reloaded manually if a change to one of the ports or the condition variable is not detected.

Client configuration

The following settings can be made:

  • Enable Client Enables or disables the client.

  • MQTT Client ID Defines the client ID that will be used for the connection.

  • MQTT Broker URL Defines the address of the broker. In addition, an individual port can be specified separated by a colon, e.g. 192.168.1.42:1234. If no port is specified, port 1883 is used by default when TLS is deactivated and port 8883 is used when TLS is activated.

  • MQTT Prefix Defines a prefix to be placed in front of each MQTT topic (e.g. {prefix}/identification ).

  • Response Topic Defines the MQTT topic on which the device publishes command response messages.

  • Keep Alive Defines the MQTT keep alive time in seconds.

  • Enable encryption (TLS) Defines whether TLS should be used for MQTT communication.

Lastwill

Allows a message to be configured that is to be sent automatically when the client disconnects from the broker. The following settings can be made:

  • Topic: Defines the topic of the message.

  • Message: Defines the content of the message.

  • QoS: Defines the QoS (Quality of Service) level at which the message is sent.

  • Retain: Sends the message with or without the retain flag.

Note

All available topics and the content of the individual messages can be found in the MQTT AsyncApi specification (see downloads at www.balluff.com on the product page).

Authentication

The following settings can be made:

  • Password: Authentication is done with password and username.

  • No authentication: The client logs on to the broker anonymously.

MQTT Message Configuration

Publishing

Among other things, the process data of the connected sensors or the status of the digital inputs and outputs can be sent via MQTT.

In the default state, all message formats described in the AsyncApi specification are sent cyclically.

This behavior can be adjusted in the MQTT Message Configuration dialog, for example so that messages are sent only when a change occurs or at a fixed interval.

../../../_images/MQTT_Narichtenkonfiguration_EN.png

MQTT Message Configuration

The following settings can be made:

General

Enables configuration of general, port-independent messages, e.g. the sender of the master identification data.

Port 1…8

Enables configuration of port-specific messages, e.g. sending the identification data of a connected IO-Link device or its process data.

../../../_images/Configure_port-specific_messages_en.png

configure port-specific messages

The following can be configured for each message to be sent:

Topic

Defines the topic under which the message is published. If the Generate topic automatically option is activated, user input is ignored and the default path specified in the AsyncApi is used.

DataType

Defines the type of message. The individual types are described in the AsyncApi specification, the operation ID listed there corresponds to the data type to be selected here.

Description

Defines a description text for the configured message. It is used only as an overview and has no other function.

Interval

Defines the fixed interval for sending a message. Either an interval or the Trigger on change option must be set.

Min. interval

Defines a minimum interval for sending between two messages.

Example:

The measured value of a connected sensor changes every millisecond. A minimum interval of 100 milliseconds is configured. This means that a message is sent every 100 milliseconds, even though the value changes more frequently.

Trigger on change

If active, a message is sent whenever a change occurs. Either this option or an interval must be set.

Note

  • Each message type can only be configured once per port.

  • The message types deviceEvents and events cannot be configured with a fixed interval.

Subscribing

In addition to the messages sent by the BNI, it is also possible to subscribe to messages from other MQTT clients. The BNI can then react to these messages, for example by changing the output state of a digital output or the process data of a connected IO-Link device.

See the AsyncApi specification for the available subscription topics and the corresponding message content. Subscription topics can be configured in the same way as publish topics.

Responses or error messages for received commands are sent to the topic configured in the Response Topic field of the MQTT Client Settings dialog.

The subscription feature is available only in fieldbus mode IoT. It is not available in other fieldbus modes.

Caution

If a subscription topic is configured, any client that can publish to this topic can send messages to the BNI and potentially change output states or process data. To protect the BNI against unauthorized access, configure access control on the MQTT broker and allow only trusted clients to send messages to the BNI.

OPC UA Server settings

To access the data, the OPC UA server must first be enabled in the Web UI. To do this, log in to the device, navigate to Settings, and click on the IoT tab. At the bottom of the page, you will find the collapsed section “OPC UA Server Settings” Open this section to enable or disable the server.

../../../_images/iiot_opcua_webui_01.png

Enable/disable OPC UA Server

Note

More information and examples can be found in chapter OPC-UA integration

REST API settings

Regarding to Rest Api, no configuration available.

Note

For detailed information how to use Rest Api, please refer to chapter REST API

IODD

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

Via the IODD dialog, device description files for IO-Link devices (IODDs) and the associated device images can be uploaded to the network module so that a more detailed illustration of the connected IO-Link devices can be provided in the Ports dialog.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

When IO-Link devices are connected and IO-Link ports are activated, the dialog shows a table with information on the IO-Link devices. The table can be updated by clicking on the refresh icon .

../../../_images/Verbundene_IO-Link-Geraete_EN.png

Connected IO-Link devices

Available IODDs

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

The available IODDs are listed under Available IODDs and can be removed by clicking on the recycle bin icon, if necessary.

../../../_images/Verfuegbare_IODDs_EN.png

Available IODDs

An IODD can be uploaded via the Choose an IODD to upload dialog between the two tab pages.

../../../_images/IODD_hochladen_EN.png

Upload IODD

In order for the automatic assignment of IODDs to connected IO-Link devices to work, the files must be named according to a specific scheme. This is done automatically in the background for IODD files. If an individual image file is selected for upload via UPLOAD FILE, which does not meet the naming requirements, a dialog will open with a corresponding message.

../../../_images/Info-Meldung_EN.png

Info message

The Connected IO-Link devices bar also displays help in the form of a list of currently connected IO-Link devices as well as the associated, required IODD file name (column IODD Filename).

Note

Always upload ZIP files with the IODD contents as provided by the IODD Finder so that all images are automatically renamed.

Firmware

Under Firmware you can see which version of the firmware is being used and when it was uploaded. Via Firmware Upload, you can upload a different firmware version. The installation starts after uploading the firmware file. Only files in bff format are supported.

You can check for firmware updates online via CHECK FOR A NEW VERSION and install an update directly.

../../../_images/Ansicht_Firmware_EN.png

Firmware view

Notifications

Clicking on the corresponding icon in the navigation bar (see chapter Navigation bar) opens the notifications.

../../../_images/Benachrichtigung_Modulzeit_EN.jpg

Notification: Module time

The notification history can be deleted with Dismiss all.

REST API

Via the REST API interface, identification data, process data and configuration settings of the network module and other connected devices can be requested and modified. The REST API interface is used by the user interface of the web interface for communication with the module.

The specification of the REST API implemented in the module is stored in YAML files in the device and can be downloaded via Help > Documents or viewed and tested via Help > Api documentation.

The present module supports the following REST APIs:

  • Generic REST API for Balluff devices and applications. Base path of the REST API in the module: http://[ip-address]/api/balluff/v1/

  • The REST API (JSON for IO-Link) standardized by the IO-Link community. Link to the official documentation (JSON for IO-Link) in the IO-Link Integration area. JSON Integration for IO-Link (ZIP file).

    Base path of the REST API in the module: http://[ip-address]/iolink/v1/

  • Detailed endpoint described in Please go to Balluff Update Platform and download the API_Description_BNI_XGx-xxx-xx5.zip file

../../../_images/iiot_api_references_01.png

BUP - Balluff Update Platform

After the product is selected, download the documentation

../../../_images/iiot_api_references_02.png

API (Rest Api) documentation including .yaml files

Note

The specification JSON for IO-Link REST API describes a functionality for process data and parameters, which requires IODD support. This functionality is also not fully implemented in the current version.

The module only supports uploading of IODDs. Writing/reading process data or parameters with their names is not supported.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

Some examples below explain how REST-API is applied.

Registration and authentication are required for some calls.

REST Login

Login is possible by entering the following address: http://[ip-address]/api/balluff/v1/users/login.

A JSON object is also specified, in which, as shown below, a user name and password are specified (see Logging in and logging out):

{
  "username": "[username]",
  "password": "[password]"
}

If the login was successful, a bearer token is returned, e.g.:

{
  "bearer": " 7euh07tdfawjej"
}

In addition, a cookie is set that must be sent with each request, e.g.:

{
  "JSESSIONID": "fgaa74a4fa2xdfg"
}

This token can now be used to perform methods that require authentication. For this, a corresponding request must be equipped with the following headers:

  • Authorization: Bearer 7euh07tdfawjej

  • Cookie: JSESSIONID fgaa74a4fa2xdfg

Requesting the device identification of the module

The device identification data of a network module can be requested via the following address:

  • http://[ip-address]/api/balluff/v1/identification

  • http://[ip-address]/iolink/v1/masters/1/identification

In the event of a successful request, an answer is supplied in the form of a JSON object with properties such as the vendorID, the serial number or the firmware revision of the respective network module.

../../../_images/BNI_Abfrage_GeraeteInfo_EN.png

Requesting the device identification

Requesting port information

All relevant configuration and status data for all IO ports of a module can be requested via:

http://[ip-address]/api/balluff/v1/ports/information

../../../_images/BNI_Abfrage_PortInfo_EN.png

Requesting the port identification

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

Device-specific parameters can be requested via the following addresses:

  • http://[ip-address]/api/balluff/v1/devices/identification

  • http://[ip-address]/iolink/v1/devices/[deviceAlias]/identification

A request via the generic REST API is the bulk version of the identical request via JSON for IO-Link.

In the case of a request via JSON for IO-Link, a deviceAlias is also specified. This corresponds to the device designation that must be configured previously. The standard device designation is Port_Xyz, with yz representing the port number (e.g. Port_X00).

In the case of successful execution, a JSON object with parameters such as vendorID, productName and applicationSpecificTag is supplied as a response.

Note

Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.

Note

A login is required to use this call (see REST Login).

Device-specific parameters for connected IO-Link devices can be set via the following address:

http://[ip-address]/iolink/v1/devices/{deviceAlias}/parameters/{index}/value

The deviceAlias corresponds to the device designation of the IO-Link device (e.g. Port_X00). The index reflects the ISDU parameter variable to be set in the IO-Link device. In the case of the applicationSpecificTag, this would be the value 24.

To set values, a JSON object must also be specified, in which corresponding parameters and values are specified as in the following example:

{ "value": [
49,
50,
51,
52,
53,
54
]}

In the case above, parameter 24 (applicationSpecificTag) was described with the ASCII string "123456".

Successful execution is not confirmed in the form of a JSON object, but with a Code 204 (Successful operation).

Setting a master parameter (sysName)

Note

A login is required to use this call (see REST Login).

A master parameter, such as SysName, can be set via the following address: http://[ip-address]/api/balluff/v1/

A JSON object with the corresponding information must also be specified:

{
  "sysName": "[SysName]"
}

Successful execution is not confirmed in the form of a JSON object, but with a Code 204 (Successful operation).

Note

If you are unable to implement your application case with the examples listed below and the information from the specifications for the REST APIs, please contact Balluff with a description of your application case.

You can find the contact details at www.balluff.com.