Startup and operation
Startup
Danger
Uncontrolled system movement
When starting up, if the network module is part of a closed loop system whose parameters have not yet been set, the system may perform uncontrolled movements. This could result in personal injury and equipment damage.
Please mind the following safety instructions:
Persons must keep away from the system’s hazardous zones.
Startup must be performed only by trained technical personnel.
Observe the safety instructions of the equipment or system manufacturer.
To start up the system, proceed as follows:
Check connections for tightness and correct polarity. Replace damaged connections.
Turn on the system.
Note
Check for the correct values, especially after replacing the BNI or after repair by the manufacturer.
Autodetect Mode
Note
Default in Fieldbus protocol: Autodetect.
Search fieldbus
As soon as the network module is initialized, it starts in autodetect mode and searches for the connected fieldbus system.
The outer port/pin LEDs light up in sequence.
Fieldbus system detected
If the fieldbus system is detected, the port/pin LEDs in a row light up green for 10 seconds. If no field bus is detected, the default address is used.
Row |
Port/Pin-LEDs of the Ports |
Meaning |
|---|---|---|
1 |
1/2 |
Profinet |
2 |
3/4 |
Ethernet/IP |
3 |
5/6 |
EtherCAT |
4 |
7/8 |
Modbus/TCP |
Note
For additional information, see Configuration guide at www.balluff.de on the product page.
Recovery Mode
In certain situations, standard configuration methods (e.g., WebUI, BET) may be inaccessible due to the following reasons:
The device is locked because the password has been forgotten.
The EtherCAT protocol has been selected on a device without a display, and the device must be reverted to standard Ethernet operation.
The IP configuration has been lost or is unknown and must be restored to default settings.
In such cases, performing a factory reset is required. As the device is not equipped with a physical push button, the procedure described below must be followed to restore the factory settings.
Before you begin
Make sure that:
The device is powered off before starting the recovery sequence.
You have access to a power supply that can provide 6 V ±0.5 V.
The device is connected through an ethernet cable to a computer.
Steps
To restore the factory settings via Recovery Mode:
Power the device with 6 V ±0.5 V at startup for about 30 seconds.
⇒ Recovery Mode is indicated by a left-to-right running light sequence on the port LEDs, illuminated in red.
Open a web browser and go to the device’s fixed IP address, 192.168.1.1 (SubNetMask 255.255.255.0).
The webserver provides exactly one page showing the factory reset option.
Note
Although the Web UI text advises using an adjustable power supply, a fixed 6 Volt supply together with a separate 24 Volt supply is also a viable alternative. Its step “1. Increase the supply voltage…” is not required — skip it and continue with the next step.
Click Factory Reset.
⇒ A dialog opens, asking to confirm the factory reset.
Confirm the dialog.
Caution
All data will be lost
All settings and configurations will be set to their factory default values.
⇒ The factory reset is executed and the device reboots.
After the reboot, power the device again with nominal voltage (24 Volt) and restart it with a power cycle.
⇒ The device is now operating with IP address 192.168.1.1 in autodetect mode.
Operation
Caution
Danger of burns from hot surfaces
The housing heats up under normal operating conditions.
There is a risk of burn injuries.
Avoid direct skin contact with the surface.
Operating notes
Regularly check function of the BNI and all associated components.
Take the BNI IO-Link master out of service whenever there is a malfunction.
Regularly check for available firmware and security updates.
Regularly review user accounts, access permissions and security-related settings.
Secure the system against unauthorized use.
Check fasteners and retighten if needed.
Cleaning
Note
For UL requirements, UL Requirements.
The product may only be cleaned when switched off.
Note
Only for BNI XG5-508-0B5-P067:
The product can be cleaned in a washdown process and is resistant to numerous alkaline, neutral and acidic cleaning media based on peroxyacids and amines with and without chlorine for the food and beverage industry.
For cleaning with Topactive OKTO, a maximum concentration of 1% is recommended. Higher concentrations may cause discoloration of the potting compound on the rear side of the device.
For further information, see ECOLAB certificate at www.balluff.com on the product page.
Maintenance
The product is maintenance-free.
Depending on the operating conditions, it may be necessary to regularly check and, if necessary, retighten the tightening torques of the plugs and caps to maintain the protection classes (see Electrical connection).