Advanced configuration
This chapter describes additional features of the OPC-UA interface. Besides the function description, step-by-step guides on how to configure those features are also included.
A way to connect to the product’s OPC UA Server is witing a Python [1] script.
Prerequisites
Laptop or PC
Python 3.10.x or 3.11.x
FreeOpcUa or AsyncUA library for Python
pip install opcua or pip install asyncua
Examples
Example 1 - SIO Port Input and Output signal state
Task: reading all SIO ports’ signal state.
Before you begin
Make sure that:
Module is powered with Us and Ua +24 Volt
The desired ports are configured as Digital In/Out (SIO mode) See I/O ports.
Port 7 - Pin2 and Pin4 (for this example) is connected to Pin 1 (+24 Volt)
Steps
To read out the SIO Input and Output signal state, the following Pytohon script should be called.
from opcua import Client
import time
client = Client("opc.tcp://192.168.1.1:4840")
client.set_user("admin")
client.set_password("your-password")
client.connect()
ports_data = [
(1, 6295, 6296), # Port 1 - Pin2, Pin4
(2, 6026, 6027), # Port 2 - Pin2, Pin4
(3, 6297, 6298), # Port 3 - Pin2, Pin4
(4, 6299, 6300), # Port 4 - Pin2, Pin4
(5, 6343, 6344), # Port 5 - Pin2, Pin4
(6, 6301, 6302), # Port 6 - Pin2, Pin4
(7, 6303, 6304), # Port 7 - Pin2, Pin4
(8, 6293, 6294), # Port 8 - Pin2, Pin4
]
# Header
print("SIO signal states of Port1..Port8")
print("")
print("-" * 24)
print(f"{'Port':<5} | {'Pin2':<6} | {'Pin4':<6}")
print("-" * 24)
# Read data and show them
for port_num, pin2_id, pin4_id in ports_data:
# Pin2
try:
val2 = client.get_node(f"ns=5;i={pin2_id}").get_value()
val2_str = str(val2).lower()
except Exception:
val2_str = "error"
# Pin4
try:
val4 = client.get_node(f"ns=5;i={pin4_id}").get_value()
val4_str = str(val4).lower()
except Exception:
val4_str = "error"
# One row in the table
print(f"{port_num:<5} | {val2_str:<6} | {val4_str:<6}")
client.disconnect()
⇒ Ruinning the script abowe will get all SIO ports’ (Port1…Port8) Pin2 and Pin4 state and write out on the consol the result. In this example the Port 7 - Pin2 and Pin4 ahould return with boolean True (1) value.
Result
SIO signal states of Port1..Port8
------------------------
Port | Pin2 | Pin4
------------------------
1 | false | false
2 | false | false
3 | false | false
4 | false | false
5 | false | false
6 | false | false
7 | true | true
8 | false | false
Example 2 - Script reading out the Information Model provided by the OPC UA server
This Python script browses the entire OPC UA Address Space (including nodes, variables, data types, and methods) and exports the server’s Information Model into a CSV file.
Terms and meanings see Summary of terms used in OPC UA
To run the script provide appropriate info for
OPC_SERVER_URL
USERNAME
PASSWORD
import asyncio
import csv
from asyncua import Client, ua
OPC_SERVER_URL = "opc.tcp://192.168.1.1:4840" # Set your IP!
USERNAME = "admin"
PASSWORD = "password" # Set your own password!
CSV_OUTPUT_FILE = "opcua_nodes_list.csv"
async def browse_recursive(node, current_path, node_list, depth=0, max_depth=8):
if depth > max_depth:
return
try:
browse_name = await node.read_browse_name()
node_class = await node.read_node_class()
node_id = node.nodeid.to_string()
display_name_obj = await node.read_display_name()
display_name = display_name_obj.Text
node_path = f"{current_path}/{browse_name.Name}" if current_path else browse_name.Name
node_list.append({
"Depth": depth,
"Path": node_path,
"Name": display_name,
"BrowseName": f"{browse_name.NamespaceIndex}:{browse_name.Name}",
"NodeId": node_id,
"NodeClass": node_class.name
})
indent = " " * depth
print(f"{indent}|-- {display_name} [{node_id}] ({node_class.name})")
# Get child references using the node-specific browse method
children_refs = await node.get_children_descriptions()
for child_ref in children_refs:
# Traverse only forward/hierarchical references downwards
child_node = client.get_node(child_ref.NodeId)
# Avoid infinite loops and skip specific system nodes
if child_ref.BrowseName.Name not in ["Server", "StaticData"]:
await browse_recursive(child_node, node_path, node_list, depth + 1, max_depth)
except Exception as e:
# Ignore errors if reading a node is restricted due to permissions
pass
async def main():
global client
print(f"Connecting to server: {OPC_SERVER_URL}...")
client = Client(url=OPC_SERVER_URL)
client.set_user(USERNAME)
client.set_password(PASSWORD)
async with client:
print("Successfully connected and authenticated!\n")
ns_array = await client.get_namespace_array()
print("--- Registered Namespaces ---")
for idx, uri in enumerate(ns_array):
print(f"NS{idx}: {uri}")
print("-" * 50 + "\n")
objects_node = client.nodes.objects
node_list = []
print("--- Browsing Address Space ---")
await browse_recursive(objects_node, "", node_list)
with open(CSV_OUTPUT_FILE, mode="w", newline="", encoding="utf-8") as f:
writer = csv.DictWriter(f, fieldnames=["Depth", "Path", "Name", "BrowseName", "NodeId", "NodeClass"])
writer.writeheader()
writer.writerows(node_list)
print(f"\nSuccess! List saved to: {CSV_OUTPUT_FILE}")
if __name__ == "__main__":
asyncio.run(main())
Result
⇒ Ruinning the script abowe will create a CSV file containing more than 500 lines, a snippet can be seen below
Depth,Path,Name,BrowseName,NodeId,NodeClass
0,Objects,Objects,0:Objects,i=85,Object
1,Objects/Locations,Locations,0:Locations,i=31915,Object
1,Objects/Aliases,Aliases,0:Aliases,i=23470,Object
2,Objects/Aliases/FindAlias,FindAlias,0:FindAlias,i=23476,Method
3,Objects/Aliases/FindAlias/InputArguments,InputArguments,0:InputArguments,i=23477,Variable
3,Objects/Aliases/FindAlias/OutputArguments,OutputArguments,0:OutputArguments,i=23478,Variable
2,Objects/Aliases/LastChange,LastChange,0:LastChange,i=32852,Variable
2,Objects/Aliases/TagVariables,TagVariables,0:TagVariables,i=23479,Object
3,Objects/Aliases/TagVariables/FindAlias,FindAlias,0:FindAlias,i=23485,Method
4,Objects/Aliases/TagVariables/FindAlias/InputArguments,InputArguments,0:InputArguments,i=23486,Variable
4,Objects/Aliases/TagVariables/FindAlias/OutputArguments,OutputArguments,0:OutputArguments,i=23487,Variable
2,Objects/Aliases/Topics,Topics,0:Topics,i=23488,Object
3,Objects/Aliases/Topics/FindAlias,FindAlias,0:FindAlias,i=23494,Method
4,Objects/Aliases/Topics/FindAlias/InputArguments,InputArguments,0:InputArguments,i=23495,Variable
4,Objects/Aliases/Topics/FindAlias/OutputArguments,OutputArguments,0:OutputArguments,i=23496,Variable
1,Objects/DeviceSet,DeviceSet,2:DeviceSet,ns=2;i=5001,Object
2,Objects/DeviceSet/DeviceFeatures,DeviceFeatures,2:DeviceFeatures,ns=2;i=15034,Object
2,Objects/DeviceSet/PlatformDevice,BNI XG5-508-1B5-Z067,3:PlatformDevice,ns=3;i=5001,Object
3,Objects/DeviceSet/PlatformDevice/DeviceManual,DeviceManual,2:DeviceManual,ns=3;i=6001,Variable
3,Objects/DeviceSet/PlatformDevice/DeviceRevision,DeviceRevision,2:DeviceRevision,ns=3;i=6002,Variable
3,Objects/DeviceSet/PlatformDevice/HardwareRevision,HardwareRevision,2:HardwareRevision,ns=3;i=6003,Variable
3,Objects/DeviceSet/PlatformDevice/Manufacturer,Manufacturer,2:Manufacturer,ns=3;i=6004,Variable
3,Objects/DeviceSet/PlatformDevice/Model,Model,2:Model,ns=3;i=6005,Variable
3,Objects/DeviceSet/PlatformDevice/RevisionCounter,RevisionCounter,2:RevisionCounter,ns=3;i=6006,Variable
3,Objects/DeviceSet/PlatformDevice/SerialNumber,SerialNumber,2:SerialNumber,ns=3;i=6007,Variable
3,Objects/DeviceSet/PlatformDevice/SoftwareRevision,SoftwareRevision,2:SoftwareRevision,ns=3;i=6008,Variable
1,Objects/NetworkSet,NetworkSet,2:NetworkSet,ns=2;i=6078,Object
1,Objects/DeviceTopology,DeviceTopology,2:DeviceTopology,ns=2;i=6094,Object
2,Objects/DeviceTopology/OnlineAccess,OnlineAccess,2:OnlineAccess,ns=2;i=6095,Variable
1,Objects/PlatformDevice,BNI XG5-508-1B5-Z067,3:PlatformDevice,ns=3;i=5003,Object
2,Objects/PlatformDevice/DeviceInfo,DeviceInfo,3:DeviceInfo,ns=3;i=5004,Object
3,Objects/PlatformDevice/DeviceInfo/BootloaderVersion,BootloaderVersion,3:BootloaderVersion,ns=3;i=6030,Variable
...
3,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1,Port1,5:Port1,ns=5;i=5016,Object
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Capabilities,Capabilities,4:Capabilities,ns=5;i=5017,Object
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Capabilities/MaxPowerSupply,MaxPowerSupply,4:MaxPowerSupply,ns=5;i=6046,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Capabilities/MaxPowerSupply/EngineeringUnits,EngineeringUnits,0:EngineeringUnits,ns=5;i=6047,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Capabilities/Pin2Support,Pin2Support,4:Pin2Support,ns=5;i=6050,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Capabilities/PortClass,PortClass,4:PortClass,ns=5;i=6051,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Capabilities/PortClass/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6052,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration,Configuration,4:Configuration,ns=5;i=5018,Object
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/ConfiguredDevice,ConfiguredDevice,4:ConfiguredDevice,ns=5;i=5019,Object
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/ConfiguredDevice/DeviceID,DeviceID,4:DeviceID,ns=5;i=6045,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/ConfiguredDevice/VendorID,VendorID,4:VendorID,ns=5;i=6062,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/CycleTime,CycleTime,4:CycleTime,ns=5;i=6044,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/Pin2Configuration,Pin2Configuration,4:Pin2Configuration,ns=5;i=6048,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/Pin2Configuration/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6049,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/PortMode,PortMode,4:PortMode,ns=5;i=6053,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/PortMode/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6054,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/ValidationAndBackup,ValidationAndBackup,4:ValidationAndBackup,ns=5;i=6060,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Configuration/ValidationAndBackup/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6061,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device,Device,5:Device,ns=5;i=5007,Object
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/DeviceID,DeviceID,4:DeviceID,ns=5;i=6019,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/General,General,4:General,ns=5;i=5009,Object
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/General/ApplicationSpecificTag,ApplicationSpecificTag,4:ApplicationSpecificTag,ns=5;i=6073,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/General/FunctionTag,FunctionTag,4:FunctionTag,ns=5;i=6075,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/General/LocationTag,LocationTag,4:LocationTag,ns=5;i=6077,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/General/ProcessDataInput,ProcessDataInput,4:ProcessDataInput,ns=5;i=6079,Variable
7,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/General/ProcessDataInput/ProcessDataLength,ProcessDataLength,4:ProcessDataLength,ns=5;i=6080,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/General/ProcessDataOutput,ProcessDataOutput,4:ProcessDataOutput,ns=5;i=6081,Variable
7,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/General/ProcessDataOutput/ProcessDataLength,ProcessDataLength,4:ProcessDataLength,ns=5;i=6082,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/HardwareRevision,HardwareRevision,2:HardwareRevision,ns=5;i=6013,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Identification,Identification,2:Identification,ns=5;i=5010,Object
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Identification/DeviceID,DeviceID,4:DeviceID,ns=5;i=6019,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Identification/ApplicationSpecificTag,ApplicationSpecificTag,4:ApplicationSpecificTag,ns=5;i=6073,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Identification/FunctionTag,FunctionTag,4:FunctionTag,ns=5;i=6075,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Identification/LocationTag,LocationTag,4:LocationTag,ns=5;i=6077,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Identification/SerialNumber,SerialNumber,2:SerialNumber,ns=5;i=6177,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Identification/VendorID,VendorID,4:VendorID,ns=5;i=6084,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Manufacturer,Manufacturer,2:Manufacturer,ns=5;i=6020,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/MinCycleTime,MinCycleTime,4:MinCycleTime,ns=5;i=6071,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/Model,Model,2:Model,ns=5;i=6072,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ParameterSet,ParameterSet,2:ParameterSet,ns=5;i=5012,Object
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ParameterSet/ApplicationSpecificTag,ApplicationSpecificTag,4:ApplicationSpecificTag,ns=5;i=6073,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ParameterSet/FunctionTag,FunctionTag,4:FunctionTag,ns=5;i=6075,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ParameterSet/LocationTag,LocationTag,4:LocationTag,ns=5;i=6077,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ParameterSet/ProcessDataInput,ProcessDataInput,4:ProcessDataInput,ns=5;i=6079,Variable
7,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ParameterSet/ProcessDataInput/ProcessDataLength,ProcessDataLength,4:ProcessDataLength,ns=5;i=6080,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ParameterSet/ProcessDataOutput,ProcessDataOutput,4:ProcessDataOutput,ns=5;i=6081,Variable
7,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ParameterSet/ProcessDataOutput/ProcessDataLength,ProcessDataLength,4:ProcessDataLength,ns=5;i=6082,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ProductID,ProductID,4:ProductID,ns=5;i=6074,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ProductText,ProductText,4:ProductText,ns=5;i=6076,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/ProfileCharacteristic,ProfileCharacteristic,4:ProfileCharacteristic,ns=5;i=6078,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/RevisionID,RevisionID,4:RevisionID,ns=5;i=6083,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/SerialNumber,SerialNumber,2:SerialNumber,ns=5;i=6177,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/SoftwareRevision,SoftwareRevision,2:SoftwareRevision,ns=5;i=6204,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/VendorID,VendorID,4:VendorID,ns=5;i=6084,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Device/VendorText,VendorText,4:VendorText,ns=5;i=6206,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/DeviceConfigurationDisabled,DeviceConfigurationDisabled,4:DeviceConfigurationDisabled,ns=5;i=6037,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Information,Information,4:Information,ns=5;i=5020,Object
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Information/ActualCycleTime,ActualCycleTime,4:ActualCycleTime,ns=5;i=6041,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Information/Baudrate,Baudrate,4:Baudrate,ns=5;i=6042,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Information/Baudrate/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6043,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Information/Quality,Quality,4:Quality,ns=5;i=6055,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Information/Quality/OptionSetValues,OptionSetValues,0:OptionSetValues,ns=5;i=6056,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Information/Status,Status,4:Status,ns=5;i=6057,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/Information/Status/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6058,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet,ParameterSet,2:ParameterSet,ns=5;i=5022,Object
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/MaxPowerSupply,MaxPowerSupply,4:MaxPowerSupply,ns=5;i=6046,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/MaxPowerSupply/EngineeringUnits,EngineeringUnits,0:EngineeringUnits,ns=5;i=6047,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Pin2Support,Pin2Support,4:Pin2Support,ns=5;i=6050,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/PortClass,PortClass,4:PortClass,ns=5;i=6051,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/PortClass/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6052,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/DeviceID,DeviceID,4:DeviceID,ns=5;i=6045,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/VendorID,VendorID,4:VendorID,ns=5;i=6062,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/CycleTime,CycleTime,4:CycleTime,ns=5;i=6044,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Pin2Configuration,Pin2Configuration,4:Pin2Configuration,ns=5;i=6048,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Pin2Configuration/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6049,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/PortMode,PortMode,4:PortMode,ns=5;i=6053,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/PortMode/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6054,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/ValidationAndBackup,ValidationAndBackup,4:ValidationAndBackup,ns=5;i=6060,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/ValidationAndBackup/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6061,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/ActualCycleTime,ActualCycleTime,4:ActualCycleTime,ns=5;i=6041,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Baudrate,Baudrate,4:Baudrate,ns=5;i=6042,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Baudrate/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6043,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Quality,Quality,4:Quality,ns=5;i=6055,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Quality/OptionSetValues,OptionSetValues,0:OptionSetValues,ns=5;i=6056,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Status,Status,4:Status,ns=5;i=6057,Variable
6,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Status/EnumStrings,EnumStrings,0:EnumStrings,ns=5;i=6058,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Pin2ProcessData,Pin2ProcessData,4:Pin2ProcessData,ns=5;i=6295,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ParameterSet/Pin4ProcessData,Pin4ProcessData,4:Pin4ProcessData,ns=5;i=6296,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/SIOProcessData,SIOProcessData,4:SIOProcessData,ns=5;i=5023,Object
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/SIOProcessData/Pin2ProcessData,Pin2ProcessData,4:Pin2ProcessData,ns=5;i=6295,Variable
5,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/SIOProcessData/Pin4ProcessData,Pin4ProcessData,4:Pin4ProcessData,ns=5;i=6296,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/HardwareRevision,HardwareRevision,2:HardwareRevision,ns=5;i=6013,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/SoftwareRevision,SoftwareRevision,2:SoftwareRevision,ns=5;i=6204,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ProductID,ProductID,4:ProductID,ns=5;i=6074,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ProductText,ProductText,4:ProductText,ns=5;i=6076,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/ProfileCharacteristic,ProfileCharacteristic,4:ProfileCharacteristic,ns=5;i=6078,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/SerialNumber,SerialNumber,2:SerialNumber,ns=5;i=6177,Variable
4,Objects/IOLinkMasterSet/BNI XG5-5x8-xB5-x067/Port1/VendorText,VendorText,4:VendorText,ns=5;i=6206,Variable
...