Diagnosis and Ident Number Reference

This chapter lists the numbers that the device reports or expects on the bus: the values of a diagnosis alarm, the error codes and their meaning, and the identification numbers (ident numbers) of all modules and submodules.

Use this chapter to look up the meaning of an alarm or error code in the PLC, or to find the ident number of a module or submodule, for example when you compare the expected and the actual configuration.

Note

All numbers are given in hexadecimal notation (0x…).

Diagnosis Alarm

The diagnosis alarm that the module generates in the event of an error is usually read out from the PLC and processed. It is also possible for the diagnosis to be read out and evaluated from the module using function modules.

IO-Link events are mapped to PROFINET diagnosis as follows:

  • An IO-Link event of type Error is reported as diagnosis with the priority Fault.

  • An IO-Link event of type Warning is reported as diagnosis with the priority Maintenance demanded.

  • An IO-Link event of type Notification (single shot) is not a diagnosis. It is reported as a process alarm (see Process Alarms).

  • A disappearing event removes the diagnosis again and generates the alarm type Diagnosis disappears.

Alarm Values

The following table lists the values that the fields of a diagnosis alarm can have.

Values of the diagnosis alarm

Field

Value

Meaning

AlarmType

0x0001
0x0002
0x0003
0x0004
0x000C

Diagnosis
Process alarm (see Process Alarms)
Pull (see Enable Pull/Plug below)
Plug (see Enable Pull/Plug below)
Diagnosis disappears

API

0x00004E01

Administrative number. The API is the same for all modules and submodules.

SlotNumber

0x0001

Slot 1, IO-Link Blocks. All slots are listed in Slots and Subslots.

SubslotNumber

0x0002 – 0x0009

Port 1 to port 8 of the port module. With the Safety Hub module, the port subslots are 0x0002, 0x0004, … 0x0010 (see Subslots of Slot 1). The subslots of all slots are listed in Slots and Subslots.

ModuleIdentNumber

–

Module in the slot, see Module Ident Numbers.

SubmoduleIdentNumber

–

Submodule in the subslot, see Submodule Ident Numbers.

User Structure Identifier

0x8000
0x8002
0x8320

Channel diagnosis (module-related errors and Safety Hub errors)
Extended channel diagnosis (IO-Link events)
Process alarm reason

ChannelNumber

0x8000

Submodule (the diagnosis refers to the entire submodule).

Priority

Fault
Maintenance demanded

IO-Link event of type Error
IO-Link event of type Warning

ChannelErrorType

–

Type of the error, see Error Codes.

ExtChannelErrorType

–

Subtype of the error. For IO-Link events it is the IO-Link EventCode, see Error Codes. The field is only available with the User Structure Identifier 0x8002.

ExtChannelAddValue

0x00000000

Not used.

The alarm types Pull and Plug are used if the port parameter Enable Pull/Plug is active (see Parameters).

Process Alarms

IO-Link events of type Notification are not reported as diagnosis. If the port parameter Enable process alarms is active (see Parameters), the device reports them as a process alarm (AlarmType 0x0002) instead.

The reason of the process alarm is coded like the error code of a diagnosis: the reason is 0x9500 or 0x9501 and the extended reason contains the IO-Link EventCode as described in IO-Link Device Events.

Error Codes

The error code of a diagnosis alarm consists of the ChannelErrorType and, for IO-Link events, the ExtChannelErrorType. The following table gives an overview of the ChannelErrorType values of the device.

ChannelErrorType overview

ChannelErrorType

Meaning

Section

0x0002

Undervoltage

Module-Related Errors

0x0003

Overvoltage

Module-Related Errors

0x0040 – 0x004B

Safety Hub: F-parameter errors

Safety Hub Errors

0x0104 – 0x0107

Actuator supply

Module-Related Errors

0x1000 – 0x1035

Safety Hub: discrepancy and short circuit errors

Safety Hub Errors

0x9500

IO-Link device events in the lower range (0x0000-0x7FFF)

IO-Link Device Events

0x9501

IO-Link device events in the upper range (0x8000-0xFFFF)

IO-Link Device Events

0x9502

IO-Link port events in the lower range (0x0000-0x7FFF)

IO-Link Port Events

Note

The BNI XG1 reports only the error types 0x0104 to 0x0107 and 0x9500 to 0x9502. The Safety Hub error types apply to the BNI XG3 and BNI XG5.

If User Structure Identifier has the value 0x8000, the module-related errors are displayed in the ChannelErrorType:

Module-related errors

ChannelErrorType

Meaning

0x0002

Undervoltage

0x0003

Overvoltage

0x0104

No actuator supply

0x0105

Undervoltage of the actuator supply

0x0106

Overvoltage of the actuator supply

0x0107

An IO-Link device is already plugged in slot 1 in the same subslot, the submodule is not used

Safety Hub Errors

The error types of the Safety Hub are available for the BNI XG3 and BNI XG5. They are reported for a connected Safety Hub (BNI IOF-329-P02-Z038 or BNI IOF-329-P02-Z092), see Integrating Safety-Hub.

F-Parameter Errors

Safety Hub F-parameter errors

ChannelErrorType

Meaning

0x0040

Mismatch of safety destination address (F_Dest_Add)

0x0041

Safety destination address not valid (F_Dest_Add)

0x0042

Safety source address not valid

0x0043

Safety watchdog time value is 0 ms

0x0044

Parameter F_SIL exceeds SIL from specific device application

0x0045

Parameter F_CRC_Length does not match the generated values

0x0046

Version of F-Parameter set incorrect

0x0047

CRC1-Fault

0x004B

Inconsistent iParameters (iParCRC error)

Input Errors

The ports are numbered as in the error text, starting with port 0. Safe inputs are available at the ports 0 to 3, 6 and 7.

Safety Hub input errors

Port

Discrepancy error

Short circuit to P, Safe_Input1

Short circuit to M, Safe_Input1

Short circuit to P, Safe_Input2

Short circuit to M, Safe_Input2

0

0x1000

0x1008

0x1010

0x1018

0x1020

1

0x1001

0x1009

0x1011

0x1019

0x1021

2

0x1002

0x100A

0x1012

0x101A

0x1022

3

0x1003

0x100B

0x1013

0x101B

0x1023

6

0x1006

0x100E

0x1016

0x101E

0x1026

7

0x1007

0x100F

0x1017

0x101F

0x1027

Output Errors

Safe outputs are available at the ports 4 and 5.

Safety Hub output errors

Port

Short circuit to P, Safe_Output

Short circuit to M, Safe_Output

4

0x102C

0x1034

5

0x102D

0x1035

The IO-Link events of a connected IO-Link device are mapped to the ChannelErrorType 0x9500 and 0x9501. The ExtChannelErrorType depends on the IO-Link EventCode:

  • 0x9500: IO-Link EventCodes 0x0000 to 0x7FFF are transferred unchanged to the ExtChannelErrorType.

  • 0x9501: IO-Link EventCodes 0x8000 to 0xFFFF are transferred to the ExtChannelErrorType with the most significant bit set to 0. For example, the EventCode 0x8C00 is reported as ExtChannelErrorType 0x0C00.

The EventCodes are defined by the IO-Link device. For the meaning of vendor-specific EventCodes, refer to the documentation of the IO-Link device.

IO-Link device events in the lower range (ChannelErrorType 0x9500)

ExtChannelErrorType (EventCode)

Error text

Help text

0x1000

General malfunction

unknown error

0x1800 – 0x180A

IO_Link EventCode 0x1800 – 0x180A

check IO-Link device manual

0x4000

Temperature fault

Overload

0x4210

Device temperature over-run

Clear source of heat

0x4220

Device temperature under-run

Insulate Device

0x5000

Device hardware fault

Device exchange

0x5010

Component malfunction

Repair or exchange

0x5011

Non volatile memory loss

Check batteries

0x5012

Batteries low

Exchange batteries

0x5100

General power supply fault

Check availability

0x5101

Fuse blown/open

Exchange fuse

0x5110

Primary supply voltage over-run

Check tolerance

0x5111

Primary supply voltage under-run

Check tolerance

0x5112

Secondary supply voltage fault (Port Class B)

Check tolerance

0x6000

Device software fault

Check firmware revision

0x6320

Parameter error

Check data sheet and values

0x6321

Parameter missing

Check data sheet

0x6350

Parameter changed

Check configuration

0x7700

Wire break of a subordinate device

Check installation

0x7701 – 0x770F

Wire break of subordinate device 1 – 15

Check installation

0x7710

Short circuit

Check installation

0x7711

Ground fault

Check installation

In the range 0x7701 to 0x770F, the number of the subordinate device is the ExtChannelErrorType minus 0x7700.

IO-Link device events in the upper range (ChannelErrorType 0x9501)

ExtChannelErrorType

IO-Link EventCode

Error text

Help text

0x0C00

0x8C00

Technology specific application fault

Reset Device

0x0C01

0x8C01

Simulation active

Check operational mode

0x0C10

0x8C10

Process variable range over-run

Process Data uncertain

0x0C20

0x8C20

Measurement range over-run

Check application

0x0C30

0x8C30

Process variable range under-run

Process Data uncertain

0x0C40

0x8C40

Maintenance required - Cleaning

Clean device

0x0C41

0x8C41

Maintenance required - Refill

Refill device

0x0C42

0x8C42

Maintenance required - Wear and tear

Exchange wear and tear parts

The events of the IO-Link port of the network module are mapped to the ChannelErrorType 0x9502. The ExtChannelErrorType is the IO-Link event code of the port (see the table below).

IO-Link port events (ChannelErrorType 0x9502)

ExtChannelErrorType (EventCode)

Error text

Help text

0x17FF

Process data mismatch

check submodule configuration

0x1800

No Device

–

0x1801

Startup parametrization error

check parameter

0x1802

Incorrect vendor ID

Inspection Level mismatch

0x1803

Incorrect device ID

Inspection Level mismatch

0x1804

Short circuit at C/Q

check wire connection

0x1805

IO-Link PHY over temperature

–

0x1806

Short circuit at L+

check wire connection

0x1807

Undervoltage at L+

check power supply (e.g. L1+)

0x1808

Device event overflow

–

0x1809

Backup inconsistency

memory out of range (2k)

0x180A

Backup inconsistency

Data storage index not available

0x180B

Backup inconsistency

Data Storage unspecific error

0x180C

Backup inconsistency

upload fault

0x180D

Backup inconsistency

download fault

0x180E

P24 (Class B) missing or undervoltage

check wire connection (e.g. L2+)

0x180F

Short circuit at P24 (Class B)

check wire connection (e.g. L2+)

0x1810

Short circuit at I/Q

check wire connection

0x1811

Short circuit at C/Q (if digital output)

check wire connection

0x1812

Overcurrent at I/Q

check load

0x1813

Overcurrent at C/Q (if digital output)

check load

0x1883

S7-PCT configuration error (wrong or not consistent parameterization)

Check parameterization

0x1888

Module defect

exchange module

0x6000

Invalid cycle time

check cycle time

0x6001

Revision fault

incompatible protocol version

0x6002

ISDU batch failed

parameter inconsistency

For example, the combination of the ChannelErrorType 0x9502 and the ExtChannelErrorType 0x1804 in an alarm of the subslot 0x0004 means: short circuit at C/Q at port 3 (X03).

Ident Numbers

PROFINET identifies the device and each of its modules and submodules by ident numbers. The PLC compares them with the configured project, and the device reports them in every alarm (see Alarm Values).

Device Identification

The device is identified by the VendorID and the DeviceID. The head module (DAP) of each product has its own ModuleIdentNumber.

Device identification

Product

Order code

VendorID

DeviceID

DAP ModuleIdentNumber

BNI XG1-505-0A5-R067

BNI00L1

0x0378

0x5500

0x00000001

BNI XG3-508-0B5-R067

BNI00L3

0x0378

0x5510

0x00000001

BNI XG3-302-1B5-Z067

BNI00L8

0x0378

0x5510

0x00000002

BNI XG3-302-0B5-R067

BNI00L7

0x0378

0x5510

0x00000003

BNI XG5-538-1B5-Z067

BNI00K7

0x0378

0x5530

0x00000001

BNI XG5-508-1B5-Z067

BNI00K6

0x0378

0x5530

0x00000002

BNI XG5-538-0B5-R067

BNI00KJ

0x0378

0x5530

0x00000003

BNI XG5-508-0B5-R067

BNI00KH

0x0378

0x5530

0x00000004

BNI XG5-508-0B5-P067

BNI00L9

0x0378

0x5530

0x00000005

BNI XG5-508-1B5-Z067-C17

BNI00ML

0x0378

0x5530

0x00000006

The tables in the following sections show the availability for these product groups:

  • XG1: BNI XG1-505-0A5-R067

  • XG3-508: BNI XG3-508-0B5-R067

  • XG3-302: BNI XG3-302-0B5-R067 and BNI XG3-302-1B5-Z067 (I/O ports without IO-Link)

  • XG5-508: BNI XG5-508-0B5-R067, BNI XG5-508-0B5-P067, BNI XG5-508-1B5-Z067 and BNI XG5-508-1B5-Z067-C17 (IO-Link Class A ports)

  • XG5-538: BNI XG5-538-0B5-R067 and BNI XG5-538-1B5-Z067 (IO-Link Class A and Class B ports)

Slots and Subslots

The device model of the device uses four slots. The slot and the subslot in an alarm locate the source of the alarm. For the structure of the device model, see Device Model.

Slots

Slot

Content

0

Head module (BNI device), PROFINET interface and Ethernet ports

1

Port modules (IO-Link I/O Ports or I/O Ports)

2

Extended Modules

3

ISDU Parameter Configuration

Subslots of Slot 0

Subslots of slot 0

Subslot

Description

0x0001

Head module (BNI device)

0x8000

PN-IO (PROFINET interface, X1)

0x8001

Port XF1 (X1 P1)

0x8002

Port XF2 (X1 P2)

Subslots of Slot 1

Subslot 0x0001 is the IO-Link Proxy (BALLUFF 8 Port IO-Link Master) and represents the network module itself. For each port, one subslot is available, starting at subslot 0x0002.

With the module IO-Link I/O Ports (w/o IO) with Safety Hub and ISDU, each port has two subslots, because a Safety Hub device uses one submodule for the secure and one for the standard communication. The port subslots are the even numbers, the following odd numbers are the Safety Hub subslots (X01.1 to X08.1).

Subslots of slot 1

Port

Subslot

Subslot with Safety Hub module: Port

Subslot with Safety Hub module: Safety Hub

IO-Link Proxy

0x0001

0x0001

–

Port 1 (X01)

0x0002

0x0002

0x0003

Port 2 (X02)

0x0003

0x0004

0x0005

Port 3 (X03)

0x0004

0x0006

0x0007

Port 4 (X04)

0x0005

0x0008

0x0009

Port 5 (X05)

0x0006

0x000A

0x000B

Port 6 (X06)

0x0007

0x000C

0x000D

Port 7 (X07)

0x0008

0x000E

0x000F

Port 8 (X08)

0x0009

0x0010

0x0011

Subslots of Slot 2

The extended modules use one subslot per submodule (Balluff Ext_Sub_Mod 1 to Balluff Ext_Sub_Mod n), starting at subslot 0x0001. The number of subslots depends on the product:

  • XG1, XG3-508, XG5-508: 16 subslots (0x0001 to 0x0010)

  • XG3-302: 13 subslots (0x0001 to 0x000D)

  • XG5-538: 17 subslots (0x0001 to 0x0011)

Subslots of Slot 3

The ISDU parameter configuration uses one subslot per port: subslot 0x0001 to 0x0008 for the ports X01 to X08. Slot 3 is not available for XG3-302.

Module Ident Numbers

The ModuleIdentNumber is part of every diagnosis alarm and identifies the module in the slot. The Class A/B variants of the XG5-538 have their own module ident numbers.

Module ident numbers

Slot

ModuleIdentNumber

Module

XG1

XG3-508

XG3-302

XG5-508

XG5-538

1

0x00004E01

IO-Link I/O Ports

1

0x00004E04

IO-Link I/O Ports (w/o IO)

1

0x0000005E

IO-Link I/O Ports (w/o IO) with Safety Hub and ISDU

1

0x00004E05

I/O Ports

1

0x00004E06

I/O Ports (w/o IO)

1

0x00005E01

IO-Link I/O Ports (Class A/B)

1

0x00005E04

IO-Link I/O Ports (w/o IO) (Class A/B)

1

0x0000505E

IO-Link I/O Ports (w/o IO) with Safety Hub and ISDU (Class A/B)

2

0x00004E03

Extended Modules

2

0x00004E07

Extended Modules

2

0x00004E09

Extended Modules

3

0x00004E02

ISDU Parameter Configuration

Submodule Ident Numbers

The SubmoduleIdentNumber is part of every diagnosis alarm and identifies the submodule in the subslot. The tables are sorted by the slot and the function of the submodule.

Slot 0

Submodule ident numbers of slot 0

SubmoduleIdentNumber

Subslot

Submodule

0x00000001

0x0001

Head module (BNI device)

0x00000002

0x8000

PN-IO (PROFINET interface)

0x00000003

0x8001

Port XF1

0x00000004

0x8002

Port XF2

Slot 1: Port Modules

The IO-Link Proxy is the fixed submodule in subslot 0x0001 of the port module.

Submodule ident numbers of the IO-Link Proxy

SubmoduleIdentNumber

Submodule

Port module

0xFFFF0000

BALLUFF 8 Port IO-Link Master

IO-Link I/O Ports

0xFFFF0004

BALLUFF 8 Port IO-Link Master

IO-Link I/O Ports (w/o IO)

0xFFFFAAAA

BALLUFF 8 Port IO-Link Master

IO-Link I/O Ports (w/o IO) with Safety Hub and ISDU

0xFFFFAAAB

BALLUFF 8 Port IO Master

I/O Ports (XG3-302)

0xFFFFAAAC

BALLUFF 8 Port IO Master

I/O Ports (w/o IO) (XG3-302)

Digital Input and Output

See Port Modules for the description of the submodules. The submodules w/o IO belong to the port modules w/o IO.

Submodule ident numbers of the digital submodules

SubmoduleIdentNumber

Submodule

Input bytes

Output bytes

0x00000081

Digital Input

1

0

0x00008100

Digital Output

0

1

0x00000082

Digital Input with IO-Link Parametrization

1

0

0x00004002

Digital Input w/o IO

0

0

0x00004001

Digital Output w/o IO

0

0

0x00004003

Digital Input with IO-Link Parametrization w/o IO

0

0

0x4FFF0000

Port deactivated

0

0

0x4FFFAAAA

Port deactivated (XG3-302)

0

0

The submodule Digital Input with IO-Link Parametrization is not available for XG3-302.

See IO-Link Generic Devices Submodules for the description of the submodules.

The SubmoduleIdentNumber of a generic IO-Link submodule is derived from the length of the input and output data (in bytes, hexadecimal):

  • Without PQI: 0x4000OOII, where OO is the number of output bytes and II is the number of input bytes.

  • With PQI: 0x0000OOII, where OO is the number of output bytes and II is the number of input bytes plus 1 (the PQI byte).

Submodule ident numbers of the IO-Link generic devices

Input bytes

Output bytes

With PQI

Without PQI

1

0

0x00000002

0x40000001

2

0

0x00000003

0x40000002

4

0

0x00000005

0x40000004

6

0

0x00000007

0x40000006

8

0

0x00000009

0x40000008

10

0

0x0000000B

0x4000000A

16

0

0x00000011

0x40000010

24

0

0x00000019

0x40000018

32

0

0x00000021

0x40000020

0

1

0x00000101

0x40000100

0

2

0x00000201

0x40000200

0

4

0x00000401

0x40000400

0

6

0x00000601

0x40000600

0

8

0x00000801

0x40000800

0

10

0x00000A01

0x40000A00

0

16

0x00001001

0x40001000

0

24

0x00001801

0x40001800

0

32

0x00002001

0x40002000

1

1

0x00000102

0x40000101

2

2

0x00000203

0x40000202

2

4

0x00000403

0x40000402

2

8

0x00000803

0x40000802

4

2

0x00000205

0x40000204

4

4

0x00000405

0x40000404

4

8

0x00000805

0x40000804

4

32

0x00002005

0x40002004

8

2

0x00000209

0x40000208

8

4

0x00000409

0x40000408

8

8

0x00000809

0x40000808

10

10

0x00000A0B

0x40000A0A

16

16

0x00001011

0x40001010

24

24

0x00001819

0x40001818

32

4

0x00000421

0x40000420

32

32

0x00002021

0x40002020

See IO-Link Devices Submodules for the description of the submodules.

Submodule ident numbers of the IO-Link devices

SubmoduleIdentNumber

Device

Input bytes

Output bytes

0xFFFF0001

BNI IOL-101-000-XXXX

1

0

0xFFFF0002

BNI IOL-102-00X-XXXX

1

0

0xFFFF0003

BNI IOL-102-S01-XXXX

2

0

0xFFFF0FFF

BNI IOL-104-00X-XXXX

2

0

0xFFFF0005

BNI IOL-104-002-X046

2

0

0xFFFF0006

BNI IOL-104-002-X046 extended

4

0

0xFFFF0007

BNI IOL-104-S02-XXXX extended with BNI IOL-104-S02-XXXX

8

0

0xFFFF0008

BNI IOL-104-S02-ZXXX extended with BNI IOL-751-VXX-K007

4

4

0xFFFF0009

BNI IOL-104-S02-RXXX extended with BNI IOL-751-VXX-K007

4

4

0xFFFF000A

BNI IOL-104-S0X-XXXX

4

0

0xFFFF000B

BNI IOL-252-000-XXXX

0

1

0xFFFF000C

BNI IOL-252-S01-XXXX

4

1

0xFFFF000D

BNI IOL-256-000-XXXX

0

2

0xFFFF000E

BNI IOL-256-S01-XXXX

7

2

0xFFFF000F

BNI IOL-302-00X-XXXX

2

2

0xFFFF0010

BNI IOL-302-002-X046

2

2

0xFFFF0011

BNI IOL-302-002-XXXX extended

4

4

0xFFFF0012

BNI IOL-302-002-X046 extended with BNI IOL-104-002-X046

4

2

0xFFFF0013

BNI IOL-302-S01-XXXX

8

2

0xFFFF0014

BNI IOL-302-S01-XXXX Input and output only

2

2

0xFFFF0015

BNI IOL-302-S01-XXXX Output only

0

2

0xFFFF0016

BNI IOL-302-S01-XXXX-C01

10

2

0xFFFF0017

BNI IOL-302-S02-XXXX

8

2

0xFFFF0018

BNI IOL-302-S02-X026

6

2

0xFFFF0019

BNI IOL-309-00X-XXXX

1

1

0xFFFF001A

BNI IOL-310-000-XXXX

2

2

0xFFFF001B

BNI IOL-355-S02-XXXX

3

1

0xFFFF001C

BNI IOL-719-002-XXXX

22

1

0xFFFF001D

BNI IOL-771-000-XXXX

2

2

0xFFFF001E

BNI IOL-772-000-XXXX

1

1

0xFFFF001F

BNI IOL-800-000-Z036

0

1

0xFFFF0020

BNI IOL-800-000-Z037

0

1

0xFFFF0021

BNI IOL-801-000-Z036

0

2

0xFFFF0022

BNI IOL-801-000-Z037

0

3

0xFFFF0023

BNI IOL-802-000-Z036

0

3

0xFFFF0024

BNI IOL-802-000-Z037

0

3

0xFFFF0025

BIS M-4XX-045

10

10

0xFFFF0026

BIS M-4XX-072

32

32

0xFFFF0027

BIS L-4XX-045

8

8

0xFFFF0028

BNI IOL-709-000-XXXX

10

0

0xFFFF0029

BNI IOL-710-000-XXXX

10

0

0xFFFF002A

BNI IOL-727-S51-XXXX

16

1

0xFFFF002B

BNI IOL-728-S51-XXXX

23

0

0xFFFF002C

BNI IOL-314-S52-P0xx

12

2

Safety Hub

See Integrating Safety-Hub for the description of the submodules. The submodules are only available for the port module IO-Link I/O Ports (w/o IO) with Safety Hub and ISDU. The secure I/O submodules are plugged in the port subslots, the other submodules are plugged in the Safety Hub subslots (see Subslots of Slot 1).

Submodule ident numbers of the Safety Hub

SubmoduleIdentNumber

Submodule

Subslot

Input bytes

Output bytes

0x00000004

BNI IOF-329-P02-Z0xx Safety I/O (PROFIsafe 2.4)

Port subslot

2 + 4 (PROFIsafe)

1 + 4 (PROFIsafe)

0x00000008

BNI IOF-329-P02-Z0xx Safety I/O (PROFIsafe 2.6)

Port subslot

2 + 5 (PROFIsafe)

1 + 5 (PROFIsafe)

0x00020002

BNI IOF-329-P02-Z0xx Standard I/O

Safety Hub subslot

1

2

0x00020003

Empty submodule

Safety Hub subslot

0

0

Slot 2: Extended Modules

See Extended Modules for the description of the submodules. The availability depends on the product group (see Device Identification).

Submodule ident numbers of the extended modules

SubmoduleIdentNumber

Submodule

Input bytes

Output bytes

XG1

XG3-508

XG3-302

XG5-508

XG5-538

0x00004500

Input Pin 4

1

0

0x00004600

Input Pin 2

1

0

0x00004700

Output Pin 4

0

1

0x00004800

Output Pin 2

0

1

0x00004900

IO-Link Device Diagnosis Disable

0

1

0x00005000

IO-Link Communication

1

0

0x00005100

IO-Link PD Valid

1

0

0x00005200

Module Diagnosis Disable

0

1

0x00005300

Pin 1 Short Circuit Detection

1

0

0x00005400

Port Event Pending

1

0

0x00005500

Pin 4/2 Actuator Warning Detection

2

0

0x00005600

IO-Link Device Event Pending

1

0

0x00005700

Pin 4/2 Actuator Ground Short Circuit Detection

2

0

0x00005800

Pin 4 IO-Link Short Circuit Detection

1

0

0x00005900

Detection for Short Circuit and Actuator Warning

1

0

0x00006000

Station Diagnosis

3

0

0x00006100

Network Module Settings

4

0

0x00006200

Outputs Pin 4 / Pin 2 - Port Mapping

0

2

0x00006300

Inputs Pin 4 / Pin 2 - Port Mapping

2

0

0x00006400

IoT Settings

5

0

0x00006500

Usermanagement Settings

9

0

0x00006600

Port Device Alias Configuration

8

0

0x00006700

Pin1 Control

0

1

Slot 3: ISDU Parameter Configuration

See ISDU Module for the description of the submodules. The submodules are available for all products except XG3-302. They have no input and no output data. The number in the name is the number of ISDU parameter entries that the submodule provides.

Submodule ident numbers of the ISDU parameter configuration

SubmoduleIdentNumber

Submodule

0x40011701

ISDU 1 Parameter

0x40011702

ISDU 4 Parameter

0x40011703

ISDU 8 Parameter

0x40011704

ISDU 16 Parameter

0x40011705

ISDU 32 Parameter

0x40011706

ISDU 64 Parameter