First steps
Before you begin
Warning
Before initial operation, please read the Safety notes.
Notice
The BNI Next Generation Family is continuously developed with new features and bug fixes. Multiple variants are part of this product family — see Supported product variants. The latest firmware, release notes, and additional files are always available on the Balluff Update Platform. Firmware can be easily updated through the integrated WebUI or the Balluff Engineering Tool.
Finding all neccesary information
Before connecting and commissioning the module, please read the safety instructions and guidelines in the manual. Always ensure that all necessary safety precautions are followed.
Accessories (to be ordered separately)
BAM01C2 - Store link
BAM01JT - Store link
BAM02K3 - Store link
Mounting the module
Warning
Additional mounting hardware required (not included)
2x M6 screws (length according to your application)
1x M4 screw for grounding point (length according to your application)
First, mount the network module at both mounting holes in its designated position using the specified torque value of max. 3 Nm. Two screws with a maximum diameter of 6 mm are required for this and not included in the box. The length can be chosen according to your application location. Next, the grounding cable must be screwed to both the module and a conductive grounding point using the included M4 screw and a specified torque value of 1.1 Nm to 1.2 Nm.
Suit moments for the installation of module and grounding cable
Main steps for installing the module:
To set up your BNI, follow these steps:
Prepare the substrate for installation
Position the module at the designated location
Screw the module in place through the two mounting holes with M6 screws
Tighten the screws to a maximum torque of 3 Nm
Attach and tighten the grounding cable with the included M4 screw and a maximum torque of 1.1 Nm to 1.2 Nm
Screw the grounding cable to the grounding point in the application
Connecting the module
When connecting the module, please follow the order described below. Always ensure that all cables are securely seated and that the plugs and cable connections are in good condition.
Main steps for connecting the module:
Plug in the M12 Ethernet cable and securely tighten the screw connection. Next, connect the unpowered 24V power cable to the module and securely tighten the screw connection. This ensures the IP67 protection class at the connections. The open connections must be covered with caps.
Then, activate the 24V power source. The module LEDs US and Link will start to light up.
In the area of the device connectors, the LEDs will form a running light in a clockwise direction, indicating the search for an active fieldbus protocol in the connected network.
Selecting the fieldbus protocol
If a supported fieldbus protocol is found in the network, the network module selects it automatically. The chosen fieldbus protocol is visualized for 10 seconds by the respective LED line in the device connector area. Until a protocol is found, the LEDs will form a running light in a clockwise direction. During this autodetection phase, the web interface is always accessible via the default IP address, where a fieldbus protocol can be selected manually. On variants equipped with a display, the fieldbus protocol can also be selected there.
Note
Autodetect cannot detect the IIoT-Mode. It must always be selected manually through the WebUI or display.
Comissioning via network and software
There are different ways to start up the module after connecting it. Accessibility via the various fieldbus protocols and interfaces varies, as shown below.
Access via PLC and fieldbus
There are different ways to put the module into operation after connecting it. The accessibility via the various fieldbus protocols and interfaces varies, as shown below.
Fieldbus |
Default IP address |
Default subnet mask |
Gateway |
|---|---|---|---|
Autodetect |
192.168.1.1 |
255.255.255.0 |
0.0.0.0 |
IIoT |
192.168.1.1 |
255.255.255.0 |
0.0.0.0 |
Profinet |
0.0.0.0 |
0.0.0.0 |
0.0.0.0 |
EtherNet/IP |
192.168.1.1 |
255.255.255.0 |
0.0.0.0 |
Modbus/TCP |
192.168.1.1 |
255.255.255.0 |
0.0.0.0 |
EtherCAT |
IP settings via EoE |
IP settings via EoE |
IP settings via EoE |
Detailed information on integrating the module via fieldbus protocols:
Access via Balluff Engineering Tool (BET)
First, download the free software Balluff Engineering Tool from the Balluff website and install it. Then, open the software and after logging in, click on “Search Devices” on the right side of the bar.
Access via browser with Web UI or the REST API
If EtherCAT was not selected as the fieldbus protocol after powering on, you can access the module via the browser and a REST interface. Use the login credentials found on the side of the module or on the included sticker. Follow these steps:
Open the URL 192.168.1.1 in your browser. You may need to change the network settings of your network adapter to the same IP range to gain access.
Log in as “admin” with the provided default password.
Open the network settings to adjust the fieldbus protocol and network settings.
To access via the REST API, open the REST documentation. There you will find all available endpoints.
Here you will find a detailed documentation of the WebUI chapter REST API.
Note
For detailed instructions, refer to the Installation and connection and Startup and operation sections.
Lost the password or IP settings and need a Factory Reset?
Please refer to chapter Recovery Mode how to get back the Factory Settings.