Register Description
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.
Index overview
Profile ID = 2
Available from Firmware 1.3.1
Index |
Description |
Access |
|---|---|---|
0 |
Profile ID (Register Mapping Version) |
RO |
1…99 |
Device (Module) Identification |
RO |
100 |
IO-Link ISDU Command Request |
RW |
300 |
IO-Link ISDU Command Response |
RO |
1100…1800 |
IO-Link Process Data Input/Output |
RO/RW |
2000 |
SIO Digital Input State |
RO |
2001 |
SIO Digital Output State |
RW |
2047 |
Digital Input State (Mirrored to 2000) |
RO |
2048 |
Digital Output State (Mirrored to 2001) |
RW |
3000 |
Device (Module&Port) Diagnostic |
RO |
3100…3800 |
IO-Link Port Diagnostic |
RO |
9100…9800 |
Port Configuration |
RW |
11000 |
Variable Processdata Register |
RW |
20000 |
Module Settings |
RW |
Note
The Register Mapping Version (list of registers, names and their content) is identified with the Profile ID which is a similar version number to HW or FW version number. Due to the content of the registers may be subject to change in the future, with keeping the compatibility and consistency, this Profile ID should be checked first when a new application is developed.
Identification
Index |
Length |
Description |
Access |
Default (example) |
|---|---|---|---|---|
0 |
1 |
Register Mapping Version (ProfileID) |
RO |
0x0001 |
1…9 |
- |
reserved |
- |
- |
10…13 |
4 |
Product Order Code (ASCII, 7 chars) |
RO |
BNI00KH |
14…29 |
16 |
Product Name (TEXT) |
RO |
BNI XG5-508-0B5-R067 |
30…99 |
- |
reserved |
- |
- |
The byte array from/to IO-Link is converted as follows in the MODBUS index:
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.
UINT16 |
LSB |
Bit(0…7) |
= IO-Link Byte[n] |
|---|---|---|---|
UINT16 |
MSB |
Bit(8…15) |
= IO-Link Byte[n+1] |
Example
The ASCII coded text of the manufacturer nameBalluff(length = 7) is converted into four (4) Word UINT16 indices as follows:
Index |
0 |
1 |
2 |
3 |
4 |
5 |
6 |
|---|---|---|---|---|---|---|---|
Byte [0…6] |
42h, |
41h, |
4Ch, |
4Ch, |
55h, |
46h, |
46h |
Word[0…3] |
4142h, |
4C4Ch, |
4655h, |
0046h |
|---|---|---|---|---|
Index |
0 |
1 |
2 |
3 |
Digital Input / Output State
When a port (X01…X08) is configured as SIO mode (Standard Input or Output) following Digital Input / Output State can be accessed.
Registers 2000, 2001 and 2047, 2048 – Digital Input / Output State
There are two register locations which can be used for Digital Input and Output. Those are working completly the same and are just mirrored location for compatibility.
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
2000 (2047) |
- |
0…7 |
Digital Input Port n Pin 4 |
BOOL |
RO |
0 = off, 1 = on |
8…15 |
Digital Input Port n Pin 2 |
BOOL |
RO |
0 = off, 1 = on |
||
2001 (2048) |
- |
0…7 |
Digital Output Port n Pin 4 |
BOOL |
R/W |
0 = off, 1 = on |
8…15 |
Digital Output Port n Pin 2 |
BOOL |
R/W |
0 = off, 1 = on |
The digital output works if the port is configured as an output.
Values – Digital Input / Output State (data)
Value |
Description |
|---|---|
0 |
off, de-energized, 0 V |
1 |
on, under power, 24 V |
Bits – Digital Input / Output State (data)
Bit |
Port n |
|---|---|
0, 8 |
X01 |
1, 9 |
X02 |
2, 10 |
X03 |
3, 11 |
X04 |
4, 12 |
X05 |
5, 13 |
X06 |
6, 14 |
X07 |
7, 15 |
X08 |
Detailed view – Digital Input / Output State (data)
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
2000 (2047) |
0 |
0 |
X01 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
1 |
X02 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
2 |
X03 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
3 |
X04 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
4 |
X05 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
5 |
X06 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
6 |
X07 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
7 |
X08 Pin4 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
1 |
0 |
X01 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
|
1 |
X02 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
2 |
X03 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
3 |
X04 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
4 |
X05 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
5 |
X06 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
6 |
X07 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
7 |
X08 Pin2 Digital Input State |
BOOL |
RO |
0 = off, 1 = on |
||
2001 (2048) |
0 |
0 |
X01 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
1 |
X02 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
2 |
X03 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
3 |
X04 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
4 |
X05 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
5 |
X06 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
6 |
X07 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
7 |
X08 Pin4 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
1 |
0 |
X01 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
|
1 |
X02 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
2 |
X03 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
3 |
X04 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
4 |
X05 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
5 |
X06 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
6 |
X07 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
||
7 |
X08 Pin2 Digital Output State |
BOOL |
RW |
0 = off, 1 = on |
IO-Link Process Data
When a port (X01…X08) is configured as IO-Link mode following Process Data Input and Output can be accessed.
There are two ways of handling the Process Data
Using fixed length 32 Bytes, accessing port-by-port allows simple, port organized access, however it requires multiple commands to perform
Using customizable variable lenght provides accessing content in one step, but pre-configuration is required
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.
Registers 1100…1800 - IO-Link Process Data (fixed length)
Read out an IO-Link port once.
Reading back the process data output is used for feedback (control).
Index |
Length |
Description |
Access |
|---|---|---|---|
1100 |
34 |
Port X01 IO-Link Process Data Input/Output |
RO |
1200 |
34 |
Port X02 IO-Link Process Data Input/Output |
RO |
1300 |
34 |
Port X03 IO-Link Process Data Input/Output |
RO |
1400 |
34 |
Port X04 IO-Link Process Data Input/Output |
RO |
1500 |
34 |
Port X05 IO-Link Process Data Input/Output |
RO |
1600 |
34 |
Port X06 IO-Link Process Data Input/Output |
RO |
1700 |
34 |
Port X07 IO-Link Process Data Input/Output |
RO |
1800 |
34 |
Port X08 IO-Link Process Data Input/Output |
RO |
Details – IO-Link Process Data 1100…1800
Index |
Length |
Description |
Access |
Value |
|---|---|---|---|---|
1n00 [5] |
1 |
Port n IO-Link Process Data Input Valid (flag) |
RO |
0 = invalid, 1 = valid |
1n01…1n16 [5] |
16 |
Port n IO-Link Process Data Input (Byte 1…32) |
RO |
– |
1n17 [5] |
1 |
Port n IO-Link Process Data Output Valid (flag) |
RW |
0 = invalid, 1 = valid |
1n18…1n33 [5] |
16 |
Port n IO-Link Process Data Output (Byte 1…32) |
RW |
– |
Note
In other words, ‘valid’ is a synonym to reliable.
For more information on Technical abbreviations and Terminology,
please refer to chapter Terminology
Port numbers – IO-Link Process Data 1100…1800
n [5] |
Port |
|---|---|
1 |
X01 |
2 |
X02 |
3 |
X03 |
4 |
X04 |
5 |
X05 |
6 |
X06 |
7 |
X07 |
8 |
X08 |
Registers 11000…11257 - Variable Processdata Registers
The registers mirror the registers 1100…1800. While the standard processdata registers are always 32-Bytes long for input and output processdata the variable processdata register adapt to the configured length.
Index |
Byte |
Name |
DataType |
Access |
Value / Description |
Note |
|---|---|---|---|---|---|---|
11000 |
0 |
IO-Link Process Data Input Valid |
UINT16 |
RO |
Each bit represents a port (Bit 0 → Port 1, etc.) |
|
1 |
Reserved |
UINT16 |
RO |
Always zero |
||
11001 |
0 |
IO-Link Process Data Output Valid |
UINT16 |
RW |
Each bit represents a port (Bit 0 → Port 1, etc.) |
|
1 |
Reserved |
UINT16 |
RW |
Write zero |
||
11002…11257 |
Variable Processdata Input/Output |
RW |
See port configuration for size and layout |
See below for Layout |
The variable processdata registers mirror the standard processdata registers (1100…1800), but adapt to the configured input/output length per port.
Input and output data lengths are defined by the port configuration.
Reserved bytes must be zero when written and will always read as zero.
If a port is not configured to IO-Link the complete processdata will be omitted in this registers (see example).
Variable Processdata Layout
The variable processdata registers are organized as follows:
Input Processdata for Ports 1–8 (read-only)
Output Processdata for Ports 1–8 (read/write)
If the configured processdata length for a port does not align to a full word (2 bytes), a padding byte is added to ensure the next port’s processdata starts at the correct word boundary.
Note
The Input Processdata section is read-only. Any write attempt will result in an error.
Section |
Port Number |
Access |
|---|---|---|
Input Processdata |
1 |
Read-only |
Input Processdata |
2 |
Read-only |
Input Processdata |
3 |
Read-only |
Input Processdata |
4 |
Read-only |
Input Processdata |
5 |
Read-only |
Input Processdata |
6 |
Read-only |
Input Processdata |
7 |
Read-only |
Input Processdata |
8 |
Read-only |
Output Processdata |
1 |
Read/Write |
Output Processdata |
2 |
Read/Write |
Output Processdata |
3 |
Read/Write |
Output Processdata |
4 |
Read/Write |
Output Processdata |
5 |
Read/Write |
Output Processdata |
6 |
Read/Write |
Output Processdata |
7 |
Read/Write |
Output Processdata |
8 |
Read/Write |
For a step-by-step guide including a worked example of the layout calculation, see Advanced configuration.
IO-Link ISDU Data
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.
For a step-by-step guide on how to read and write ISDU data, see Advanced configuration.
Registers 100, 300 – Acyclic Command Channel (including ISDU Read/Write Request)
Index |
Length |
Description |
Access |
Default |
|---|---|---|---|---|
100 |
4…121 |
IO-Link ISDU Command Request |
RW |
- |
300 |
5…122 |
IO-Link ISDU Command Response |
RO |
- |
Details – Registers 100…220 Command Request Channel = ISDU Read/Write Request
Index |
Byte |
Name |
Data Type |
Access |
Needed? |
Value |
|---|---|---|---|---|---|---|
100 |
- |
Command |
UINT16 |
RW |
M [1] |
1 = read, 2 = write |
101 |
- |
Port No. |
UINT16 |
RW |
M [1] |
1…8 |
102 |
- |
Index |
UINT16 |
RW |
M [1] |
0…0xFFFF |
103 |
- |
Subindex |
UINT16 |
RW |
M [1] |
0…255 |
104 [3] |
- |
Data Length [Byte] |
UINT16 |
RW |
O [2] |
1…232 |
105…220 [4] |
0 |
Data Byte n |
UINT8 |
RW |
O [2] |
- |
105…220 [4] |
1 |
Data byte n1 |
UINT8 |
RW |
O [2] |
- |
Details - Registers 300…421 Command Response Channel = ISDU Read/Write Response
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
300 |
- |
- |
Command (last sent) |
UINT16 |
RO |
1 = read, 2 = write |
301 |
- |
- |
Port No. |
UINT16 |
RO |
1…8 |
302 |
- |
- |
Index |
UINT16 |
RO |
0…0xFFFF |
303 |
- |
- |
Subindex |
UINT16 |
RO |
0…255 |
304 |
- |
- |
Error Code |
UINT16 |
RO |
0 = no error other values = see Tab. 6-15 |
305 |
- |
Data Length [Bytes] |
UINT16 |
RO |
1…232 |
|
306…421 |
0 |
- |
Data Byte n |
UINT8 |
RO |
- |
306…421 |
1 |
- |
Data Byte n+1 |
UINT8 |
RO |
- |
Error codes
Error Code |
Description |
|---|---|
0x0000 |
No error, command was successful |
0x4001 |
ARGBLOCK_NOT_SUPPORTED |
0x4002 |
ARGBLOCK_INCONSISTENT |
0x4003 |
DEVICE_NOT_SUPPORTED |
0x4004 |
SERVICE_NOT_AVAILABLE |
0x4005 |
DEVICE_NOT_IN_OPERATE |
0x4006 |
MEMORY_OVERRUN |
0x4011 |
PORT_NUM_INVALID |
0x4034 |
ARGBLOCK_LENGTH_INVALID |
0x4036 |
SERVICE_TEMP_UNAVAILABLE |
0x8000…0x80FF |
IO-Link error code from the connected device, see IO-Link specification |
Diagnostic
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.
Index |
Length |
Description |
Access |
|---|---|---|---|
3000 |
10 |
Module and Port Diagnostic |
RO |
3100 |
10 |
X01 IO-Link Info & Events |
RO |
3200 |
10 |
X02 IO-Link Info & Events |
RO |
3300 |
10 |
X03 IO-Link Info & Events |
RO |
3400 |
10 |
X04 IO-Link Info & Events |
RO |
3500 |
10 |
X05 IO-Link Info & Events |
RO |
3600 |
10 |
X06 IO-Link Info & Events |
RO |
3700 |
10 |
X07 IO-Link Info & Events |
RO |
3800 |
10 |
X08 IO-Link Info & Events |
RO |
Details – Diagnostic
Registers 3000…3009 – Module and Port Diagnostic
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
3000 |
0 |
0…3 |
reserved |
– |
RO |
– |
3000 |
0 |
4 |
Sensor Voltage Short Circuit |
BOOL |
RO |
– |
3000 |
0 |
5 |
Actuator Short Circuit |
BOOL |
RO |
– |
3000 |
0 |
6 |
Actuator Warning |
BOOL |
RO |
– |
3000 |
0 |
7 |
IO-Link Short Circuit |
BOOL |
RO |
– |
3001 |
0 |
0…7 |
Port n: IO-Link Communication Established |
BOOL |
RO |
– |
3001 |
1 |
8…15 |
Port n: IO-Link PD Input Valid |
BOOL |
RO |
– |
3002 |
0 |
0…7 |
Port n: IO-Link Valid Device Connected |
– |
– |
– |
3002 |
1 |
8…15 |
reserved |
– |
– |
– |
3003 |
– |
– |
reserved |
– |
– |
– |
3004 |
0 |
0…7 |
Port n: Actuator shutdown (Pin 2) |
BOOL |
RO |
– |
3004 |
1 |
8…15 |
Port n: Actuator shutdown (Pin 4) |
BOOL |
R |
– |
3005 |
0 |
0…7 |
Port n: Actuator Warning (Pin 2) |
BOOL |
RO |
– |
3005 |
1 |
8…15 |
Port n: Actuator Warning (Pin 4) |
BOOL |
RO |
– |
3006 |
– |
– |
reserved |
– |
– |
– |
3007 |
– |
– |
reserved |
– |
– |
– |
3008 |
– |
– |
reserved |
– |
– |
– |
3009 |
– |
– |
reserved |
– |
– |
– |
BOOL value |
Meaning |
|---|---|
0 |
false, status not available |
1 |
true, status available |
Bit |
Port n |
|---|---|
0, 8 |
X01 |
1, 9 |
X02 |
2, 10 |
X03 |
3, 11 |
X04 |
4, 12 |
X05 |
5, 13 |
X06 |
6, 14 |
X07 |
7, 15 |
X08 |
Registers 3010…3080 – IO-Link Port Diagnostic
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.
Detailed information about the connected IO-Link device.
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
|---|---|---|---|---|---|---|
3n00 [5] |
0 |
0 |
IO-Link Mode |
BOOL |
RO |
– |
1 |
Device Connected |
BOOL |
RO |
– |
||
2 |
Valid PD IN Data |
BOOL |
RO |
– |
||
3 |
Wrong Vendor ID or Device ID |
BOOL |
RO |
– |
||
4 |
Wrong Cycle Time |
BOOL |
RO |
– |
||
5 |
Wrong Length PD IN |
BOOL |
RO |
– |
||
6 |
Wrong Length PD OUT |
BOOL |
RO |
– |
||
7 |
reserved |
– |
RO |
– |
||
1 |
– |
reserved |
– |
RO |
– |
|
3n01 [5] |
– |
– |
Vendor ID |
UINT16 |
RO |
– |
3n02 [5] |
0 |
– |
Device ID (MSB) |
UINT8 |
RO |
– |
1 |
– |
reserved |
– |
RO |
– |
|
3n03 [5] |
– |
– |
Device ID (LSB) |
UINT16 |
RO |
– |
3n04 [5] |
0 |
– |
Entry #1 Event Qualifier |
IOL coded |
RO |
IOL coded |
1 |
– |
reserved |
– |
RO |
– |
|
3n05 [5] |
– |
– |
Entry #1 Event Code |
UINT16 |
RO |
IOL coded |
3n06 [5] |
0 |
– |
Entry #2 Event Qualifier |
Enum |
RO |
IOL coded |
1 |
– |
reserved |
– |
RO |
– |
|
3n07 [5] |
– |
– |
Entry #2 Event Code |
UINT16 |
RO |
IOL coded |
3n08 [5] |
0 |
– |
Entry #3 Event Qualifier |
Enum |
RO |
IOL coded |
1 |
– |
reserved |
– |
RO |
– |
|
3n09 [5] |
– |
– |
Entry #3 Event Code |
UINT16 |
RO |
IOL coded |
Port numbers – Registers 3010…3080
n [5] |
Port |
|---|---|
1 |
X01 |
2 |
X02 |
3 |
X03 |
4 |
X04 |
5 |
X05 |
6 |
X06 |
7 |
X07 |
8 |
X08 |
IOL coded Event Qualifier – Registers 3010…3080
Bit |
Description |
|---|---|
0…2 |
Instance |
3 |
Source |
4…5 |
Type |
6, 7 |
Mode |
Configuration
Registers 9100…9800 – Port Configuration
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.
Index |
Length |
Name |
|---|---|---|
9100 |
7 |
X01 Port Configuration |
9200 |
7 |
X02 Port Configuration |
9300 |
7 |
X03 Port Configuration |
9400 |
7 |
X04 Port Configuration |
9500 |
7 |
X05 Port Configuration |
9600 |
7 |
X06 Port Configuration |
9700 |
7 |
X07 Port Configuration |
9800 |
7 |
X08 Port Configuration |
Please see the following tables for information on the structure of the port configuration.
Index |
Byte |
Bit |
Name |
Data Type |
Access |
Value |
Note |
|---|---|---|---|---|---|---|---|
9n00 [6] |
0 |
– |
Master Cycle Time |
UINT8 |
RW |
IO-Link coded |
|
1 |
– |
reserved |
– |
– |
|||
9n01 [6] |
0 |
– |
Pin 2 Port Mode |
UINT8 |
RW |
0 = deactivated
1 = Digital Input
2 = Digital Output
|
|
1 |
– |
Pin 4 Port Mode |
UINT8 |
RW |
0 = deactivated
1 = IOL Manual
2 = IOL Autostart
3 = Digital input
4 = Digital Output
|
||
9n02 [6] |
0 |
– |
Validation ID |
UINT8 |
RW |
0 = No device check
1 = Compatible V1.0
2 = Compatible V1.1
3 = Backup Restore
4 = Restore
|
|
1 |
– |
reserved |
– |
– |
– |
||
9n03 [6] |
– |
– |
Vendor ID |
UINT16 |
RW |
– |
|
9n04 [6] |
0 |
– |
Device ID (MSB) |
UINT8 |
RW |
– |
|
1 |
– |
reserved |
– |
– |
– |
||
9n05 [6] |
– |
– |
Device ID (LSB) |
UINT16 |
RW |
– |
|
9n06 [6] |
– |
– |
Input Processdata Length |
UINT16 |
RW |
0…32 |
|
9n07 [6] |
– |
– |
Output Processdata Length |
UINT16 |
RW |
0…32 |
Notes
Note
Automatic Shutdown of Pin 1 Power on Port Deactivation:
If a port is configured to deactivate Pin 2 and Pin 4, the power supply on Pin 1 is automatically shut down.
Port numbers – Registers 9100…9800
n [5] |
Port |
|---|---|
1 |
X01 |
2 |
X02 |
3 |
X03 |
4 |
X04 |
5 |
X05 |
6 |
X06 |
7 |
X07 |
8 |
X08 |
Coding of the master cycle time of the IO-Link specification
Note
Please check whether IO-Link is supported by your module before using this function. For more information on product variants that support IO-Link, see Supported product variants.
Time Base Encoding |
Time Base Value |
Calculation |
Cycle Time |
|---|---|---|---|
0 |
0.1 ms |
Multiplier × Time base |
0.4…6.3 ms |
1 |
0.4 ms |
6.4 ms + Multiplier × Time Base |
6.4…31.6 ms |
10 |
1.6 ms |
32.0 ms + Multiplier × Time Base |
32.0…132.8 ms |
11 |
reserved |
reserved |
reserved |
Register 20000 - Module Settings
Note
This setting is only available for the XG5-538-…-variants.
Global configuration registers for the Module (Device).
Index |
Byte |
Bit |
Name |
DataType |
Access |
Value |
|---|---|---|---|---|---|---|
20000 |
Output Powerloss Behavior |
UINT16 |
RW |
See below |
The parameter defines what happens to active outputs on Pin 2 and Pin 4 when UA voltage is lost. The configured setting is saved permanently — it can be written once and will be retained after a power reset.
Value 0 – US Outputs shutdown on UA powerloss
All active outputs on Pin 2 and Pin 4 are automatically switched off in the event of a UA voltage drop. This matches the behavior of a XG5-508-… master, even though Pin 2 and Pin 4 of Class A output ports are supplied by US, and Pin 4 of Class B ports are supplied by UA.
Value 1 – Hardware Defined
US powered outputs will not be switched off in the event of a UA voltage drop. All outputs remain in their current state. Only Class B Pin 2 outputs are physically supplied by UA and will therefore be shut down.