About this guide
Validity
This guide provides all the information required for the safe use of the BTL magnetostrictive linear position sensor (measurement system) with SSI interface.
It applies to the following models (see Type code):
BTL BNC _ 00 - _ _ _ _ - C15DU _ _ _ - _ _ _ _ _ _
BTL ZNC _ 00 - _ _ _ _ - C15DU _ _ _ - _ _ _ _ _ _
Read this guide and the other applicable documents completely before installing and operating the product.
Original User’s guide
This guide was created in English. Other language versions are translations of this guide.
© Copyright 2026, Balluff GmbH
Zabergäustraße 8, 73765 Neuhausen auf den Fildern
All contents are protected by copyright. All rights reserved, including the right to reproduce, publish, edit and translate this document.
Other applicable documents
Additional information about this product can be found at www.balluff.com on the product page, e.g. in the following documents:
Data sheet
Declaration of Conformity
Disposal
Symbols and conventions
Individual actions are indicated by a preceding triangle.
Instruction 1
Action sequences are numbered consecutively:
Instruction 1
Instruction 2
Note
Note, tip
This symbol indicates general notes.
Explanation of the warnings
Always observe the warnings in this guide and the measures described to avoid hazards.
The warnings used here contain various signal words and are structured as follows:
SIGNAL WORD
Type and source of the hazard
Consequences if not complied with
Measures to avoid hazards
The individual signal words mean:
Notice
Identifies a danger that could damage or destroy the product.
Caution
The general warning symbol together with the signal word CAUTION indicates a hazard which can lead to slight or moderate injuries.
Warning
The general warning symbol together with the signal word WARNING indicates a hazard which can lead to death or serious injuries.
Danger
The general warning symbol in conjunction with the signal word DANGER identifies a hazard which, if not avoided, will certainly result in death or serious injury.
Abbreviations
- AdSS:
Adjustable Switching Sensor
- BET:
Balluff Engineering Tool
- FMM:
Flexible Magnet Mode
- IODD:
IO-Device-Description
- ISDU:
IO-Link-Parameter (Index Service Data Unit)
- LSB:
Least Significant Bit
- MSB:
Most Significant Bit
- PD:
Process Data
- PDV:
Process Data Variable