Reset Commands

Description

The device supports various reset commands for resetting the set parameters to default values. Each of these commands is accessed by means of System Commands.

This function is defined in the IO-Link specification and is implemented according to Version 1.1.4.

ISDU

Reset Commands – ISDU

Name

Index

Subindex

Access

Length

Data Type

Data Storage

Default

System Commands

0x0002 (2)

0

W

1 byte

UINT8

n/a

–

System Commands

Reset Commands – System Commands

Command Value

Device Action

0x80 (128)

Device Reset – Device Reset means a warm start of the device. During this process, the microcontrollers are restarted and all initializations performed again without any change made to the parameter values.

0x81 (129)

Application Reset – This reset is performed using IO-Link specification V1.1.4.

  • Resets all parameters and device settings to default values (with the exception of the identification and tagging parameters)

  • No reset of the configuration of the device variant

  • Set DS-Upload request (accept the data in the memory)

  • No communication stop or restart

0x82 (130)

Restore Factory Settings – This reset is performed using IO-Link specification V1.1.4.

  • Reset all parameters and device settings to default settings (including identification and tagging parameters)

  • Reset the configuration of the device variants to the default variant

  • No DS-upload-request

  • No communication stop or restart

0xA5 (165)

Maintenance Reset – Resets all resettable maintenance and service life parameters for the user so that the next maintenance cycle can begin.