The identification data is used for the identification and management of the IO-Link devices.
ISDU
Identification – ISDU
Name
Index
Sub-index
Access
Length
Data Type
Data Storage
Default
Vendor Name
0x0010 (16)
R
7 bytes
STRING
n/a
“Balluff”
Vendor Text
0x0011 (17)
R
15 bytes
STRING
n/a
“www.balluff.com”
Product Name
0x0012 (18)
R
≤ 64 bytes
STRING
n/a
“BTL BNCA00-xxxx-C15DUxxx-000S32”
Product ID
0x0013 (19)
R
≤ 64 bytes
STRING
n/a
“BTL BNCA00-xxxx-C15DUxxx-000S04”
Product Text
0x0014 (20)
R
≤ 64 bytes
STRING
n/a
Balluff Position Transducer
Serial Number
0x0015 (21)
R
16 bytes
STRING
n/a
Hardware Revision
0x0016 (22)
R
2 bytes
STRING
n/a
Firmware Revision
0x0017 (23)
R
≤ 10 bytes
STRING
n/a
Application Specific Tag
0x0018 (24)
R/W
≤ 32 bytes
STRING
Yes
“***“
Function Tag
0x0019 (25)
R/W
≤ 32 bytes
STRING
Yes
“***“
Location Tag
0x001A (26)
R/W
≤ 32 bytes
STRING
Yes
“***“
Product Type Code
0x0700 (1792)
R
≤ 64 bytes
STRING
n/a
e.g. “BTL BNCA00-0500-C15DUA01- 000S32”
Product Order Code
0x0701 (1793)
R
7 bytes
STRING
n/a
e.g. “BTLxxxx”
Application Specific Tag
With the Application Specific Tag parameter, a string (maximum 32 bytes) can be written to the device. This value typically describes the application in which the product is used.
Function Tag
With the Function Tag parameter, a string (maximum 32 bytes) can be written to the device. This value typically describes the function of the product in the application area.
Location Tag
With the Location Tag parameter, a string (maximum 32 bytes) can be written to the device. This value typically describes the location of the product in the application area.
Product Type Code
The Balluff type code is stored permanently in the device.
Product Order Code
The Balluff order code is stored permanently in the device.