Parameter Manager
Description
The parameter manager is responsible for the saving of parameters in the permanent memory of the device. On startup, all stored parameters are read from permanent memory; if parameters are changed, the data is stored within the permanent memory by the parameter manager.
All data is protected with a CRC32 checksum. In the event of damaged memory, the parameter manager outputs the Parameters not consistent event.