Profile Characteristic

Description

Profile Characteristic is a readable parameter that provides information about which IO-Link profiles are supported. It is used mainly to allow profile function modules of the control unit to detect which profile or functions on the device are available.

This parameter is defined in the IO-Link specification.

ISDU

Profile Characteristic – ISDU

Name

Index

Subindex

Access

Length

Data Type

Data Storage

Default

Profile Characteristic

0x000D (13)

0

R

6 bytes (Smart Sensor Profile Ed. 2), 8 bytes (Smart Sensor Profile Legacy), 6 bytes (Smart Sensor Profile Legacy, without PDIn)

UINT16[]

n/a

–

The parameter can be read via subindex 0 and consists of multiple profile indices and function classes (each 16-bit values).

If a profile ID is specified, this means that all included function classes are supported. If only sub-functions are supported, these are output explicitly as an individual function class.

This device supports the following profiles:

Profile Characteristic – supported profiles

Profile ID

Name / Description

0x0001

Smart Sensor Profile Legacy

0x000B

Digital Measuring Sensor

0x0030

BLOB

0x0031

Firmware Update

0x4000

Common Profile

The following function classes are supported:

Profile Characteristic – supported function classes

Function Class ID

Name / Description

0x8000

Device Identification

0x8002

Process Data Mapping

0x8003

Device Diagnosis

0x8004

Teach Commands

0x800B

Measurement High Resolution

0x8100

Extended Identification

All individual functions are described in this guide.

For more exact descriptions of the profiles, refer to the corresponding profile specifications (see www.io-link.com).