Internal Temperature

Description

The device has internal temperature monitoring. This records the device temperature as well as the maximum and minimum values since production and since the last time the device was restarted.

An upper and a lower threshold value can be defined for the device temperature module. If the threshold is exceeded or if device limit values are exceeded or undercut, the device triggers IO-Link events.

Note

The internal device temperature is measured in the device and is therefore higher than the ambient temperature. The level of this increased temperature depends on the ambient temperature, the ventilation of the device and the device settings.

Process Data

Internal temperature – Process data

Object ID

Name

Description

Direction

0x004E (78)

Temperature Status Customer Limits

Temperature status – Warning related to the configured customer limits [Index 0x0053]. Set when out of limits.

Input

0x004F (79)

Temperature Status Device Limits

Temperature status – Warning related to the device limits. Set when out of limits.

Input

0x0050 (80)

Device Temperature

Current device temperature in °C.

Input

ISDU

Internal temperature – ISDU (overview)

Name

Index

Subindex

Access

Length

Data Type

Data Storage

Default

Device Temperature

0x0052 (82)

0

R

10 bytes

**n/a*

Device Temperature

1

R

2 bytes

INT16

n/a

–

Minimum Device Temperature Since Reset

2

R

2 bytes

INT16

n/a

–

Maximum Device Temperature Since Reset

3

R

2 bytes

INT16

n/a

–

Lifetime Minimum Device Temperature

4

R

2 bytes

INT16

n/a

–

Lifetime Maximum Device Temperature

5

R

2 bytes

INT16

n/a

–

Device Temperature Alarm Configuration

0x0053 (83)

0

R/W

4 bytes

Yes

Lower Alarm Level Device Temperature

1

R/W

2 bytes

INT16

No

−40

Upper Alarm Level Device Temperature

2

R/W

2 bytes

INT16

No

115

Device Temperature

Device Temperature contains information about the device temperature (current value in °C), the minimum or maximum device temperature since the last time the device was switched on/reset (in °C) and minimum or maximum device temperature during the lifetime of the device (in °C).

Device Temperature Alarm Configuration

Setting of the lower threshold value (in °C) for the device temperature warning (0x8D20) and of the upper threshold value (in °C) for the device temperature warning (0x8D10).

Events

Internal temperature – Events

Event Code

Event Type

Event – Description – Remedy

Device Status

0x4000 (16384)

Error

Temperature Fault – Overload – The device is operated outside of the device-specific temperature limits. Risk of device damage.

4 – Failure

0x4210 (16912)

Warning

Device Temperature Overrun – Clear Heat Of Source – Risk of device damage. The device is too hot. Remove heat source, provide the device with heat insulation if necessary.

2 – Out-of-specification

0x4220 (16928)

Warning

Device Temperature Underrun – Insulate Device – Risk of device damage. The device is too cold. Insulate the device.

2 – Out-of-specification

0x8D10 (36112)

Warning

Device Temperature Upper Warning – The set upper temperature warning threshold has been exceeded.

0 – Device is operating properly.

0x8D20 (36128)

Warning

Device Temperature Lower Warning – The device temperature has fallen below the set lower temperature warning threshold.

0 – Device is operating properly.