Signal Delay

Description

This is a function that is applied to an internal binary signal. This function allows the user to apply time delay functions to the internal binary signal of the device (On-Delay, Off- Delay, One-Shot or On/Off-Delay).

Mathematics/Algorithm

Process Data

Signal delay – process data

Object ID

Name

Description

Direction

0x0008 (8)

Signal Delay Channel 1

Output signal Signal Delay Channel 1

Input

0x0009 (9)

Signal Delay Channel 2

Output signal Signal Delay Channel 2

Input

0x000A (10)

Signal Delay Channel 3

Output signal Signal Delay Channel 3

Input

0x000B (11)

Signal Delay Channel 4

Output signal Signal Delay Channel 4

Input

../../../_images/Signal_Delay_with_text.png

ISDU

Signal delay – ISDU

Name

Index

Subindex

Access

Length

Data Type

Data Storage

Default

Signal Delay Input

0x0096 (150)

0

R/W

8 bytes

Yes

Channel 1

1

R/W

2 bytes

UINT16(ENUM)

No

0

Channel 2

2

R/W

2 bytes

UINT16(ENUM)

No

0

Channel 3

3

R/W

2 bytes

UINT16(ENUM)

No

0

Channel 4

4

R/W

2 bytes

UINT16(ENUM)

No

0

Signal Delay Mode

0x0097 (151)

0

R/W

4 bytes

Yes

Channel 1

1

R/W

1 byte

UINT8(ENUM)

No

0

Channel 2

2

R/W

1 byte

UINT8(ENUM)

No

0

Channel 3

3

R/W

1 byte

UINT8(ENUM)

No

0

Channel 4

4

R/W

1 byte

UINT8(ENUM)

No

0

Signal Delay On-Delay

0x0098 (152)

0

R/W

8 bytes

Yes

Channel 1

1

R/W

2 bytes

UINT16

No

0

Channel 2

2

R/W

2 bytes

UINT16

No

0

Channel 3

3

R/W

2 bytes

UINT16

No

0

Channel 4

4

R/W

2 bytes

UINT16

No

0

Signal Delay Off-Delay / One-Shot

0x0099 (153)

0

R/W

8 bytes

Yes

Channel 1

1

R/W

2 bytes

UINT16

No

0

Channel 2

2

R/W

2 bytes

UINT16

No

0

Channel 3

3

R/W

2 bytes

UINT16

No

0

Channel 4

4

R/W

2 bytes

UINT16

No

0

Signal Delay Status

0x009A (154)

0

R

4 bytes

n/a

Channel 1

1

R

1 byte

UINT8(ENUM)

n/a

–

Channel 2

2

R

1 byte

UINT8(ENUM)

n/a

–

Channel 3

3

R

1 byte

UINT8(ENUM)

n/a

–

Channel 4

4

R

1 byte

UINT8(ENUM)

n/a

–

Signal Delay Input Parameter

With Signal Delay Input, the internal binary signal source can be selected. Input contains a list of the internal binary signals.

Signal Delay Mode Parameter

With Signal Delay Mode, the current mode of the signal delay function can be selected.

Signal Delay – Signal Delay Mode

Value

Meaning

Description

0x00 (0)

Deactivated

Deactivated

0x01 (1)

Delay

On, Off and On-/Off delay function

0x02 (2)

One-Shot

One-Shot function

Signal Delay On-Delay Parameter

With Signal Delay On-Delay, the time for On-Delay can be set. The value represents the time in milliseconds. The value range is between 0x0000 (0) and 0xFFFF (65535). A value of 0x0000 (0) represents no delay. The parameter has no effect in One-Shot-Modus.

Signal Delay Off-Delay / One-Shot Parameter

With Signal Delay Off-Delay / One-Shot, the time for Off-Delay and One-Shot can be set. The value represents the time in milliseconds. The value range is between 0x0000 (0) and 0xFFFF (65535). A value of 0x0000 (0) represents no delay.

Signal Delay Status Parameter

With Signal Delay Status, the current status of each channel can be read.

Signal Delay – Signal Delay Status

Value

Meaning

Description

0x00 (0)

Off

Output signal of Signal Delay = 0/FALSE

0x01 (1)

On

Output signal of Signal Delay = 1/TRUE

0x02 (2)

On-Delay

Output signal of Signal Delay = 0/FALSE and On-Delay currently running.

0x03 (3)

Off-Delay

Output signal of Signal Delay = 1/TRUE and OFF-Delay currently running.

0x07 (7)

One-Shot

Output signal of Signal Delay = 1/TRUE and One-Shot function currently running.

0xFF (255)

Deactivated

Feature is deactivated.

System Commands

Signal delay – System Commands

Command Value

Device Action

0x81 (129)

Application Reset – Resets writable parameters to the default value.

0x82 (130)

Restore Factory Settings – Resets writable parameters to the default value.