Skip to content

Troubleshooting#

This section helps you diagnose the most common RadarImager problems without repeating the full setup and configuration guides. Start with the symptom that best matches your issue, then follow the linked detailed guide.

  • The image result looks wrong


    Object not visible, wrong layer, poor contrast, mirrored display, blur, ghosting, and shadows.

    Image result issues

  • Streaming or parameter behavior is unexpected


    Frame drops, MTU / GenDC issues, non-persistent settings, and changes that only apply after a new measurement.

    Streaming & configuration issues

Quick triage#

If you are not sure where to start, check the following in order:

  1. Power and status
    • The Power LED and Status LED show normal operation.
    • The Ethernet cable and trigger wiring are connected to the intended ports.
  2. Network and connection
  3. Acquisition
    • A trigger event actually occurs.
    • useExternalTrigger and the trigger mode are configured correctly.
  4. Image content
    • The object is inside the configured image range.
    • The correct layer is selected and the normalization is suitable.
  5. Performance and persistence
    • No frame drops occur.
    • You are aware that some changes require a new measurement and that configuration is not persistent after restart.

Symptom overview#