Image Result Issues#
Use this page if an image is acquired, but the result is not useful yet. This includes missing objects, cropped objects, wrong layers, poor contrast, mirrored views, blur, shadows, and ghost images.
The object is not visible or is cropped#
Typical symptoms:
- The image updates, but the object is missing.
- Only part of the object is visible.
- The object appears too early or too late in the image.
Check the following measurement parameters first:
- Set
objectLengthXlarge enough so the full object fits into the image. - Start with
offsetDistanceX=0 mmto make sure the object appears at all. - Set
distanceZToDeepestLayerOfInterestlarge enough so the object is inside the acquired depth range. - Verify
reverseObjectMovementDirectionXif the conveyor runs opposite to the default direction.
Important:
- Changes to
objectLengthX,distanceZToDeepestLayerOfInterest, andreverseObjectMovementDirectionXonly take effect after a new measurement. - The quick-start strategy in Generate First Image is the fastest way to make the object visible first and optimize later.
The image looks empty, too dark, or shows the wrong layer#
Typical symptoms:
- The image is almost black.
- The object is only visible in some layers.
- The displayed layer does not match the expected depth.
Check the following:
- Navigate through the stack with
layerSelection.indexes. - Use
normalAbs.kind=GLOBALto quickly find strong reflections. - After finding the relevant layer, switch back to
LAYERfor detailed inspection. - Verify that
distanceZToDeepestLayerOfInterestis not limiting the selectable layers too much.
Useful references:
The image has poor contrast or details are hard to recognize#
Typical symptoms:
- The object is visible, but important details are lost.
- The image is too dark, too bright, or unstable between measurements.
Check the following:
- For quick inspection, use dynamic normalization with
normalAbs.kind=LAYERorGLOBAL. - For reproducible results or manual normalization fine-tuning, configure
PREDEFINEDtogether withnormalAbs.minPredefinedValandnormalAbs.maxPredefinedVal. - Use
normalAbs.logScaleandnormalAbs.dynamicsif weak and strong reflections should be visible together. - If the issue is only the displayed orientation, check
transpose,flip.dim_1, andflip.dim_2.
Useful references:
The image is distorted, blurry, or contains ghost images#
Typical symptoms:
- The object appears stretched or compressed in movement direction.
- The image contains shadows or multiple object contours.
- The object shape twists or smears.
Most common causes:
objectSpeedXis inaccurate.reverseObjectMovementDirectionXis set incorrectly.- The RadarImager is misaligned mechanically.
- The selected layer is not the actual layer of interest.
Use this order:
- Verify that the correct layer is selected.
- Check the movement direction setting.
- Recheck the configured object speed.
- Inspect the mounting alignment.
Detailed follow-up guides: