Process Data Profile Selection |
|
|
|
0x1850 (6224) |
Notification |
Process data profile selection cannot be used – default value is used. |
0 – Device is operating properly. |
0x1851 (6225) |
Notification |
Process Data Update Timeout – For information purposes only. A PDinput has been delayed over an extended period of time. |
0 – Device is operating properly. |
0x1852 (6226) |
Warning |
Multiple Process Data Update Timeout – For information purposes only. A PDinput has been delayed over an extended period of time. |
0 – Device is operating properly. |
Device Temperature |
|
|
|
0x4000 (16384) |
Error |
Temperature Fault – Overload – The device is operated outside of the device-specific temperature limits. Risk of device damage. |
4 – Failure |
0x4210 (16912) |
Warning |
Device Temperature Overrun – Clear Heat Of Source – Risk of device damage. The device is too hot. ► Remove heat source, provide the device with heat insulation if necessary. |
2 – Out-of-Specification |
0x4220 (16928) |
Warning |
Device Temperature Underrun – Insulate Device – Risk of device damage. The device is too cold. ► Insulate the device. |
2 – Out-of-Specification |
0x8D10 (36112) |
Warning |
Customer-defined upper warning for device temperature. The upper threshold value for the temperature warning has been exceeded. |
0 – Device is operating properly. |
0x8D20 (36128) |
Warning |
Customer-defined lower warning for device temperature. The lower threshold value for the temperature warning has been dropped below. |
0 – Device is operating properly. |
Signal Quality |
|
|
|
0x8CFF (36095) |
Warning |
Low signal quality level |
Out-of-Specification |
Balluff Measurement Sensor Profile |
|
|
|
0x8D00 (36096) |
Warning |
The measurement value is below the measurement range. Accuracy cannot be guaranteed. |
2 – Out of Specification |
0x8D01 (36097) |
Warning |
The measurement value is above the measurement range. Accuracy cannot be guaranteed. |
2 – Out of Specification |
0x8D02 (36098) |
Warning |
The measurement value is below the detection range; no measurement value can be determined. ► Check application. |
2 – Out of Specification |
0x8D03 (36099) |
Warning |
The measurement value is above the detection range; no measurement value can be determined. ► Check application. |
2 – Out of Specification |
0x8D04 (36100) |
Warning |
No measurement value can be determined. ► Check application. |
2 – Out of Specification |
0x8D05 (36101) |
Warning |
Measurement error / redundancy check failed. ► Check application. |
2 – Out of Specification |
Electrical monitoring |
|
|
|
0x5110 (20752) |
Warning |
Primary supply voltage exceeded. ► Check for deviations in the supply. |
2 – Out-of-Specification |
0x5111 (20753) |
Warning |
Primary supply voltage below minimum value. ► Check for deviations in the supply. |
2 – Out-of-Specification |
0x8D0B (36107) |
Warning |
Overload or short circuit at pin 2. ► Check wiring. |
2 – Out-of-Specification |
0x8D0D (36109) |
Warning |
Incorrect load/cable breakage, analog current output pin 2. ► Check wiring or connected devices. |
2 – Out-of-Specification |
0x8D15 (36117) |
Warning |
Overload at pin 2. ► Check wiring. |
2 – Out-of-Specification |
Parameter manager |
|
|
|
0x8D24 (36132) |
Notification |
An error occurred during the EEPROM write – for information only. |
0 – Device is operating properly. |
0x8D25 (36133) |
Error |
Parameters not consistent – basic settings are used, service required. Parameterization processes and resets can no longer be performed. |
4 – Failure |
0x8D26 (36134) |
Warning |
User data was reset to the default settings. ► Check settings and acknowledge warning. |
1 – Maintenance required |
Switching profiles |
|
|
|
0x8DC0 (36288) |
Notification |
Teach-in Timeout – The current teach-in process took too long and was interrupted. |
0 – Device is operating properly. |