Variant Configuration

Description

The device variant can be changed either via ISDU with this parameter or by using the IO-Link compatibility mode. If this parameter is written, the device variant is not changed immediately but instead after the device is restarted. If the device variant is changed via the IO-Link compatibility mode, the change in this parameter is visible immediately.

This parameter is not changed by a reset.

Hint

After a variant changeover, an inconsistent configuration may occur because there is no automatic changeover of parameters.

It is therefore recommended that the setup be done in the following order:

  1. Variant setting

  2. Activate the variant with a device restart.

  3. Check parameters and set valid parameters if necessary or use Data Storage (see section Data Storage).

The variant dependent functional differences are described in the Radar frontend section.

ISDU

Name Index Subindex Access Length Data Type Data Storage Default
Device Variant 0x0055 (85) 0 R/W 2 bytes UINT16(ENUM) No 0x01

Device Variant

This parameter indicates which variant is currently set.

The following device variants are available:

Value

Description

Device Id

0x01 (1)

Distance/ Object detection

0x0C0102

(786690)

0x02 (2)

Radar Reflex Gate

0x0C0103

(786691)