Measurement Profiles

Description

The sensor realizes the measuring Smart Sensor Profile Ed. 2 according to profile SSP 4.2.2. The profile defines four different ranges in which a measurement value (Measurement Value) can be output:

  • The measurement range (Measurement Range)

  • Detection range (Detection Range)

  • Out of Range

  • No Measurement Data

The evaluation is realized based on the value “Transducer Value High Resolution” (PDObjectID 0x0025) as the distance output provided by the Radar Frontend, see Radar frontend.

Ranges for which a measurement value is output

Ranges for which a measurement value is output

Measurement Range

Within the measurement range, all values specified in the data sheet related to measurement accuracy are satisfied. Information on the size of the measurement range can be found in parameter MDC Descriptor, which contains the lower measurement limit (Lower Limit) and upper measurement limit (Upper Limit).

Detection Range

Outside of the measurement range, a measurement value output in the non-linear areas (Limited Accuracy Areas) is still possible, though the accuracy cannot be ensured for these areas. Limited accuracy is indicated via the Measurement Warning bit in the process data.

Out of Range

Outside of the detection range, the sensor can determine whether the measurement value is below or above the detection range. A meaningful measurement value is not possible in these areas. Instead, a replacement value is output:

Out of Range

Status

Value

Out of Range Minus

–2,147,483,640 (0x80000008)

Out of Range Plus

2,147,483,640 (0x7FFFFFF8)

In addition to the replacement value, the Measurement Error bit is set.

No Measurement Data

If no measurement value can be determined, the replacement value No Measurement Data is output:

No Measurement Data

Status

Value

No Measurement Data

2,147,483,644 (0x7FFFFFFC)

In addition to the replacement value, the Measurement Error bit is set.

This state is set if no target can be detected within the measurement range. See more details in Radar frontend.

Process Data

Object ID

Name

Description

Direction

0x0028 (40)

Measurement Value (Distance)

Distance measurement value.

Input

0x002A (42)

Measurement Scale (Distance)

The scaling as the exponent of a power of ten

Input

0x002B (43)

Measurement Error

Measurement value outside of the detection range or no measurement value

Input

0x002C (44)

Measurement Warning

Measurement value outside of the measurement range

Input

0x0171 (369)

Measurement Value (Target Strength)

Target Strength value.

Input

0x0172 (370)

Measurement Scale (Target Strength)

The scaling as the exponent of a power of ten

Input

Measurement Value

The current measurement value as signed, 32-bit number. In case of an error, a substitute value is output (see Out of Range and No Measurement Data).

Measurement Scale

The scaling value is a signed, 8-bit number. The scaling indicates the exponents of a power of ten of the measurement value relative to the base unit meter in case of Distance, and dB in case of Target Strength. This value is used to interpret the unit of the output value.

Note

Measurement Value [unit] of output value = SI unit × 10Measurement Scale

Measurement Error

Indicates if the measurement value is outside of the detection range or if no measurement value can be determined.

Measurement Warning

Indicates if the measurement value is outside of the measurement range.

Process Data Profiles

PDin

Process Data
Byte 11 Byte 10 Byte 9 Byte 8 Byte 7 Byte 6 Byte 5 Byte 4 Byte 3 Byte 2 Byte 1 Byte 0
MDC1 (Target Distance) MDC1 Scale Status and Switching Signal Channels MDC2 (Target Strength) MDC2 Scale Switching Signal Channels
Status and Switching Signal Channels
Bit 7 Bit 6 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0
System error Measurement Error Measurement range warning Signal Quality [^1] Switching Signal Channel 1.2 Switching Signal Channel 1.1
[^1]: Signal Quality bit is available only in Distance/ Object detection variant
Switching Signal Channels
Bit 7 Bit 6 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0
Switching Signal Channel 2.2 Switching Signal Channel 2.1

ISDU and Reset Behavior

Name Index Subindex Access Length Data Type Data Storage Default
Measurement Data Channel Descriptors
MDC1 Descriptor 0x4080 (16512) 0 R 11 bytes n/a
Lower Limit 1 R 4 bytes INT32 n/a 300
Upper Limit 2 R 4 bytes INT32 n/a 15000
Unit Code 3 R 2 bytes UINT16(ENUM) n/a 1010 (m)
Scale 4 R 1 byte INT8 n/a -3
MDC2 Descriptor 0x4081 (16513) 0 R 11 bytes n/a
Lower Limit 1 R 4 bytes INT32 n/a 0
Upper Limit 2 R 4 bytes INT32 n/a 64
Unit Code 3 R 2 bytes UINT16(ENUM) n/a 1383 (dB)
Scale 4 R 1 byte INT8 n/a 0
Measurement Channel configuration (only for Distance measurement value)
Hide Limited Accuracy Areas 0x00C0 (192) 0 R/W 1 byte UINT8(ENUM) Yes 0
Measurement Offset 0x00C1
(193)
0 R/W 4 bytes INT32 Yes 0
Measurement Preset 0x00C2
(194)
0 R/W 4 bytes INT32 Yes 0
Measurement Output Characteristics 0x00C3
(195)
0 R/W 1 byte BOOL Yes 0
Measurement Hysteresis 0x00C4 (196) 0 R/W 4 bytes UINT32 Yes 0
Measurement Range 0x0202 (514) 0 R/W 8 bytes Yes
Lower Limit 1 R/W 4 bytes INT32 300 mm
Upper Limit 2 R/W 4 bytes INT32 15000 mm

MDC Descriptor

The MDC Descriptor contains information about the current value range of the measurement value (Measurement Value) within the limits of the measurement range (Measurement Range), about the unit and the scaling of the measurement value. The values for the lower measurement limit (Lower Limit) and upper measurement limit (Upper Limit) specify the value range.

The Scale parameter in the MDC Descriptor is a signed 8 bit number. The scaling indicates the exponents of a power of ten of the measurement value relative to the base unit. The basic unit is coded by the parameter Unit Code in the MDC Descriptor. The possible unit values of the sensor include:

Unit

Value

Meter

1010

Decibel

1383

On delivery, the lower measurement value limit has its origin at value 300. If an offset is set, the value of the lower measurement value limit changes according to the Measurement Offset.

Hide Limited Accuracy Areas

Measurement values are still displayed outside the measuring range. These do not conform to the limits specified in the data sheet. The output of the non-linear area (Limited Accuracy Areas) can be configured. If the output is deactivated (Hidden), the sensor outputs either Out Of Range Plus or Out Of Range Minus if the measurement range is exited.

Value

Meaning

0x00 (0)

Visible

0xFF (255)

Hidden

Measurement Offset

The Measurement Offset is subtracted from the current measurement value. This parameter can be reset using Application Reset and Factory Reset.

Measurement Preset

Measurement Preset can be used to calculate a Measurement Offset. Measurement Preset specifies a target value that should be achieved after a Teach Preset by the current measurement value. Following a successful Teach Preset, the current measurement value has the same value as Measurement Preset.

This parameter can be reset using Application Reset and Factory Reset.

Measurement Output Characteristics

The Measurement Output Characteristics parameter defines the output characteristic, which can be rising or falling. This setting affects the offset setting. It is possible that the offset setting needs to be performed again after this setting is changed.

This parameter can be reset using Application Reset and Factory Reset.

Value

Meaning

0x00 (0)

Falling

0xFF (255)

Rising

Measurement Hysteresis

The hysteresis of the measurement value can be set with parameter Measurement Hysteresis. This parameter is used to dampen unstable measurement values. This parameter can be reset using Application Reset and Factory Reset.

Measurement Range

With Measurement Range, the measurement range can be changed by teaching with the Teach Lower Limit and Teach Upper Limit System Commands or by overwriting the parameter.

This parameter Measurement Range can be reset using Application Reset and Factory Reset.

System Commands

Command Value

Device Action

0xE0 (224)

Teach Preset – Sets the current measurement value to the value of Measurement Preset.

0xE1 (225)

Teach Lower Limit – Sets the lower end of the measurement range.

0xE2 (226)

Teach Upper Limit – Sets the upper end of the measurement range.

For an overview of all System Commands, see section System Commands.

Events

Event Code

Event Type

Event – Description – Remedy

Device Status

0x8D00 (36096)

Warning

The measurement value is below the measurement range. Accuracy cannot be guaranteed.

2 – Out of Specification

0x8D01 (36097)

Warning

The measurement value is above the measurement range. Accuracy cannot be guaranteed.

2 – Out of Specification

0x8D02 (36098)

Warning

The measurement value is below the detection range; no measurement value can be determined.

► Check application.

2 – Out of Specification

0x8D03 (36099)

Warning

The measurement value is above the detection range; no measurement value can be determined.

► Check application.

2 – Out of Specification

0x8D04 (36100)

Warning

No measurement value can be determined.

► Check application.

2 – Out of Specification

0x8D05 (36101)

Warning

Measurement error/redundancy check failed.

► Check application.

2 – Out of Specification