Internal Temperature

Description

The device has internal temperature monitoring. This records the device temperature as well as the maximum and minimum values since production and since the last time the device was restarted.

An upper and a lower threshold value can be defined for the device temperature module. If the threshold is exceeded or if device limit values are exceeded or undercut, the device triggers IO-Link events.

Note

The internal device temperature is measured in the device and is therefore higher than the ambient temperature. The level of this increased temperature depends on the ambient temperature, the ventilation of the device and the device settings.

Process Data

Object ID

Name

Description

Direction

0x004E (78)

Temperature Status Customer Limits

Temperature status – Warning related to the configured customer limits [Index 0x0053]. Set when out of limits.

Input

0x004F (79)

Temperature Status Device Limits

Temperature status – Warning related to the device limits. Set when out of limits.

Input

0x0050 (80)

Device Temperature

Current device temperature in °C.

Input

ISDU

Name Index Subindex Access Length Data Type Data Storage Default
Internal Temperature 0x0052 (82) 0 R 10 bytes n/a
Internal Temperature 1 R 2 bytes INT16 n/a –
Internal Temperature Min (Since last Start) 2 R 2 bytes INT16 n/a –
Internal Temperature Max (Since last Start) 3 R 2 bytes INT16 n/a –
Internal Temperature Min (Lifetime) 4 R 2 bytes INT16 n/a –
Internal Temperature Max (Lifetime) 5 R 2 bytes INT16 n/a –
Internal Temperature Alarm Configuration 0x0053 (83) 0 R/W 4 bytes Yes
Internal Temperature Lower Threshold 1 R/W 2 bytes INT16 -10°C
Internal Temperature Upper Threshold 2 R/W 2 bytes INT16 75°C

Internal Temperature

Internal Temperature contains information about the device temperature (current value in °C), the minimum or maximum device temperature since the last time the device was switched on/reset (in °C) and minimum or maximum device temperature during the lifetime of the device (in °C).

Internal Temperature Alarm Configuration

Setting for the lower threshold value (in °C) for the device temperature warning (0x8D20) and upper threshold value (in °C) for the device temperature warning (0x8D10).

Events

Event Code

Event Type

Event – Description – Remedy

Device Status

0x4000 (16384)

Error

Temperature Fault – Overload – The device is operated outside of the device-specific temperature limits. Risk of device damage.

4 – Failure

0x4210 (16912)

Warning

Device Temperature Overrun – Clear Heat Of Source – Risk of device damage. The device is too hot.

► Remove heat source, provide the device with heat insulation if necessary.

2 – Out-of-Specification

0x4220 (16928)

Warning

Device Temperature Underrun – Insulate Device – Risk of device damage. The device is too cold.

► Insulate the device.

2 – Out-of-Specification

0x8D10 (36112)

Warning

Customer-defined upper warning for device temperature. The upper threshold value for the temperature warning has been exceeded.

0 – Device is operating properly.

0x8D20 (36128)

Warning

Customer-defined lower warning for device temperature – The lower threshold value for the temperature warning has been dropped below.

0 – Device is operating properly.