Pin Configuration Assignment

Description

Several internal digital and analog signals are available that can be output at the pins of the device. Pin 4 and pin 2 can be configured with the following functions:

Pin 4

  • Digital Output

Pin 2

  • Digital Output

  • Analog Output

ISDU

Name Index Subindex Access Length Data Type Data Storage Default
Pin 4 Function 0x0090
(144)
0 R/W 2 bytes Yes
Behavior IO-Link 1 R/W 1 byte UINT8
(ENUM)
0x00 (0)
IO-Link
Mode 2 R/W 1 byte UINT8
(ENUM)
0x00 (0)
Inactive
Pin 4 Digital Configuration¹ 0x0091 (145) 0 R/W 4 bytes Yes
Signal Source 1 R/W 2 bytes UINT16
(ENUM)
0x003F (63)
Switching Signal Channel 1.1
Logic 2 R/W 1 byte UINT8
(ENUM)
0x00 (0) Normal
Type 3 R/W 1 byte UINT8
(ENUM)
0x02 (2)
Push-Pull
Pin 2 Function 0x0093 (147) 0 R/W 2 bytes Yes
Behavior IO-Link 1 R/W 1 byte UINT8
(ENUM)
0x01 (1)
Normal Operation
Mode 2 R/W 1 byte UINT8
(ENUM)
0x00 (0)
Inactive
Pin 2 Digital Configuration¹ 0x0094
(148)
0 R/W 4 bytes Yes
Signal Source 1 R/W 2 bytes UINT16
(ENUM)
0x003F (63)
Switching Signal Channel 1.1
Logic 2 R/W 1 byte UINT8
(ENUM)
0x00 (0)
Normal
Type 3 R/W 1 byte UINT8
(ENUM)
0x00 (0)
PNP
Pin 2 Analog Configuration² 0x0095
(149)
0 R/W 4 bytes Yes
Signal Source 1 R/W 2 bytes UINT16
(ENUM)
0x0028 (40)
Target distance
Characteristic 2 R/W 1 byte UINT8
(ENUM)
0x00 (0)
Rising
Type 3 R/W 1 byte UINT8
(ENUM)
0x00 (0)
4..20mA

¹ The settings in the digital configuration are only used if the pin was configured as a digital output or digital input.

² The settings in the analog configuration are only used if the pin was configured as an analog output.

With Behavior IO-Link, the behavior of the pins during active IO-Link communication can be determined. The pin can either continue to perform its function or become inactive.

Pin 4

Value

Name

Description

0x00 (0)

IO-Link

This is the communication pin. It cannot execute any other function during an active IO-Link connection.

Pin 2

Value

Name

Description

0x00 (0)

Inactive

The pin has no function and is high-impedance.

0x01 (1)

Normal Operation

The pin retains its function.

Mode

The function of the pin can be selected with Mode.

Pin 4

Value

Name

Description

0x00 (0)

Inactive

The pin has no function and is high-impedance.

0x01 (1)

Digital Output

The pin works as a digital output.

Pin 2

Value

Name

Description

0x00 (0)

Inactive

The pin has no function and is high-impedance.

0x01 (1)

Digital Output

The pin works as a digital output.

0x02 (2)

Analog Output

The pin works as an analog output.

Signal Source

With Signal Source, the internal signal source for the pin can be selected. Various signal sources are available that can be output or read on a pin.

Digital

Value

Name

Description

0x0000 (0)

Nothing

No Signal Source

0x0017 (23)

Primary supply voltage under-run

Power supply voltage is under its limit.

0x0018 (24)

Primary supply voltage over-run

Power supply voltage is over its limit.

0x002B (43)

MDC Measurement Error

No valid Target found.

0x002C (44)

MDC Out of Measurement Range Warning

Target out of the configured measurement range.

0x002F (47)

System Error

A System Error is active.

0x003F (63)

Switching Signal Channel 1.1

The state of Switching Signal Channel 1.1.

0x0040 (64)

Switching Signal Channel 1.2

The state of Switching Signal Channel 1.2.

0x0173 (371)

Switching Signal Channel 2.1

The state of Switching Signal Channel 2.1.

0x0174 (372)

Switching Signal Channel 2.2

The state of Switching Signal Channel 2.2.

0x004E (78)

Device Temperature Alarm Status

The Device Temperature Alarm is active.

Analog

Value

Name

Description

0x0028 (40)

Target distance

The current Target distance.

0x0171 (369)

Target strength

The current Target strength.

Logic

With Logic, the input/output can be configured as inverted or normal.

Value

Name

Description

0x00 (0)

Normal

Non-inverting logic

0x01 (1)

Inverted

Inverted logic

Characteristic

With Characteristic, a rising or falling characteristic of the analog output can be configured.

Value

Name

Description

0x00 (0)

Rising

Rising input value = Rising output value

0x01 (1)

Falling

Rising input value = Falling output value

Type

The output can be configured with Type.

Digital

Value

Name

Description

0x00 (0)

PNP

PNP output

0x01 (1)

NPN

NPN output

0x02 (2)

Push-Pull

Push-Pull output

Analog

Value

Name

Description

0x00 (0)

4…20mA

Analog current output 4 to 20mA

0x01 (1)

0…20mA

Analog current output 0 to 20mA

0x02 (2)

1…5V

Analog voltage output 1 to 5V

0x03 (3)

0…10V

Analog voltage output 0 to 10V

0x04 (4)

2…10V

Analog voltage output 2 to 10V

Warning

The voltage and current settins listed above (e.g., 4…20mA, 0…10V) only represent the nominal signal ranges of the configured meassurement range, not the absolute maximum or minimum values that may occur. Actual output may exceed these ranges in error or out-of-range conditions. More information about the analog output configuration can be found in the Analog Output section.