Signal Quality

Description

The signal quality is specified in percent steps as a value between 0 and 100%. If the signal quality cannot be provided, a substitute value of 0xFF (255) is output. The threshold value for the monitoring function can be set and is used to define two states of the signal quality. The signal quality is considered to be good at or above the threshold value; the signal quality is considered to be bad below the threshold value. A state change from good to bad signal quality triggers the Low Signal Quality Level IO-Link event.

The output of the current signal quality can provide support both when setting up as well as during predictive maintenance. When setting up, the location, the orientation and the environmental conditions can be adapted to achieve a satisfactory signal quality level. If the signal quality is checked regularly, a deterioration of the performance can be preventatively combated.

In addition, the monitoring of the signal quality offers an immediate response in the event of a critical failure. This reaction is triggered if the signal quality drops below the adjustable threshold value and gives the all clear if a satisfactory signal quality level is once again achieved.

The signal status is indicated by LED (see section LED Meaning).

The function can be deactivated by setting the threshold value to zero.

Mathematics/Algorithm

The signal quality value is based on the Target Strength signal. If the Target Strength is below a defined lower threshold (3dB), the signal quality is set to 0%. If the Target Strength is above an upper threshold (20dB), the signal quality is set to 100%. For values in between, the function linearly maps the Target Strength to a percentage between 0% and 100%.

Process Data

Object ID

Name

Description

Direction

0x0021 (33)

Signal Quality Bad

Output of the current signal quality evaluation;

TRUE means a signal quality below the threshold value, FALSE means a signal quality equal to or above the threshold value.

Input

Also see section Process Data Profiles.

ISDU

Name Index Subindex Access Length Data Type Data
Storage
Default
Low Signal Quality Threshold 0x00CE (206) 0 R/W 1 byte UINT8 Yes 0
Signal Quality 0x00CF (207) 0 R 2 bytes n/a
Current Signal Quality 1 R 1 byte UINT8 n/a –
Signal Quality Bad 2 R 1 bit BOOL n/a –

Low Signal Quality Threshold

The threshold value for low signal quality can be set in order to monitor the current signal quality. It is displayed as a value between 0 and 100 in percent. If the current signal quality value drops below the signal quality threshold value, the Low Signal Quality Level warning is output.

The function can be deactivated by setting the threshold value to zero.

Current Signal Quality

The current signal quality is displayed as a value between 0 and 100 in percent. If no valid signal quality is available, the value is set to 255.

Signal Quality Bad

The status of the signal quality is displayed as a Boolean value. If the value is TRUE, the signal quality is below the threshold value; if the value is FALSE, the signal quality is equal to or greater than the threshold value.

System Commands

Command

Value

Device Action

0x81 (129)

Application Reset – Sets the threshold value with ISDU index 0xCE Low Signal Quality Threshold to default 0. The feature is thereby deactivated and the evaluation of index 0xCF subindex 2 always results in FALSE.

0x82 (130)

Restore Factory Settings – Sets the threshold value with ISDU index 0xCE Low Signal Quality Threshold to default 0. The feature is thereby deactivated and the evaluation of index 0xCF subin dex 2 always results in FALSE.

For an overview of all System Commands, see section System Commands.

Events

Event Code

Event Type

Event – Description – Remedy

Device Status

0x8CFF

(36095)

Warning

Low signal quality level

2 – Out-of Specification

Variant Dependence

The functionality is available only in Distance/ Object detection variant.