Process Data Info and Configuration

Description

Process data information and configuration offers various possibilities related to process data:

  • Selection of a process dataset specified by the device

  • Information about the structure of the input and output data

  • Information about the last valid value for input and output data

As a diagnosis function, monitoring of the updates of certain process values is available. If these are not updated in the specified time, the device sends corresponding diagnosis messages.

Invalid Process Data

Input data (from the device to the master) is only marked as invalid if the device has the Failure device status.

Info

In the case of individual pieces of faulty data, the data is not marked as invalid but is instead replaced by substitution values or error codes. This is to be taken into account during the evaluation.

ISDU

Name Index Subindex Access Length Data Type Data Storage Default
Process Data Profile Selection 0x0051 (81) 0 R/W 1 byte UINT8(ENUM) Yes 0x01
Process Data Input Descriptor 0x000E (14) 0 R 21 bytes UINT8[] n/a –
Last Valid Process Data Inputs 0x0028 (40) 0 R 12 bytes – n/a –

PD Profile Selection

There is only one PD Profile

PD Description

This parameter is used to specify the structure of the currently selected process data profile for input and output data. The individual process data variables are described.

The total list is accessible via subindex 0, a single entry is possible using a specific subindex. Subindex 1 corresponds to the least significant (or the element most recently transferred in the process data stream). When reading out the entire list, this element is transferred first.

The length of the list is dependent on which process data profile is selected. A single element has a length of 3 bytes.

Byte number Contents Values
Byte 1 Data type 0: OctetStringT
1: Set of BoolT
2: UIntegerT
4: Float32T
5…255: reserved
Byte 2 TypeLength 0…255 bits
Byte 3 Bit offset 0…255 bits

Last Valid Process Data

This parameter indicates the most recently valid input or output data of the device. The first transferred byte in the process data (MSB) is transferred first. This is an exact representation. Access occurs via subindex 0.

Events

PD Update Timeout

With special process data values, the device automatically checks whether the values are updated in the time period specified by the device. If an update timeout is triggered as a result, this is output via the following diagnosis messages:

Event Code Event Type Event – Description – Remedy Device Status
0x1851 (6225) Notification Process Data Update Timeout – for information purposes only. A PDinput has been delayed over an extended period of time. 0 – Device is operating properly.
0x1852 (6226) Warning Multiple Process Data Update Timeout – for information purposes only. A PDinput has been delayed over an extended period of time. 0 – Device is operating properly.

PD Profile Selection after Change of Variant

If the variant of the device is changed, the currently set profile is retained.

In the case that the corresponding PD profile is not valid for this variant, the default profile for the corresponding variant is selected.

Event Code Event Type Event – Description – Remedy Device Status
0x1850 (6224) Notification Process data profile selection cannot be used – default value is used. 0 – Device is operating properly.

Variant Dependence

There is no variant dependency in PD-Profiles. All variants use the same PD-profile.

PD Invalid

PD Inputs Invalid:

Input data (device-to-master) is marked as invalid if the device status (see section Device Status and Detailed Device Status of the device is Failure. In all other states, replacement values for the data are output for which the content cannot be output correctly).