Flexible mode
Description
The following chapters are relevant, in case the Flexible mode mode has been selected via the SmartLight control feature.
The flexible mode gives the possibility to the user to define separate colors for all of the LED levels independently. Each LED level may have Color A and Color B defined by an ISDU parameter. Both colors can be set as an RGB value. The color for each LED level can be set to Color A or Color B by toggling a process data bit.
Output Process Data
Note
Only mode dependent bytes are described in these chapter.
Byte |
Description |
|---|---|
Byte 0…3 |
Defined by other primary device functions |
Byte 4 |
|
Byte 5 |
|
Byte 6 |
|
Byte 7…xx |
Not used in this mode |
Output process data bitfield descriptions
LED 1…8 control
Bit |
Description |
|---|---|
Bit 0 |
|
Bit 1 |
|
Bit 2 |
|
Bit 3 |
|
Bit 4 |
|
Bit 5 |
|
Bit 6 |
|
Bit 7 |
Note
LED 5 … 8 are available only for BNI IOL-811-205-K03x and BNI IOL-812-205-K03x
LED 9…16 control
Bit |
Description |
|---|---|
Bit 0 |
|
Bit 1 |
|
Bit 2 |
|
Bit 3 |
|
Bit 4 |
|
Bit 5 |
|
Bit 6 |
|
Bit 7 |
Note
LED 9 … 12 are available only for BNI IOL-811-205-K03x and BNI IOL-812-205-K03x
LED 13 … 20 are available ony for BNI IOL-812-205-K03x
LED 17…20 control
Bit |
Description |
|---|---|
Bit 0 |
|
Bit 1 |
|
Bit 2 |
|
Bit 3 |
|
Bit 4…7 |
Reserved |
Note
LED 9 … 12 are available only for BNI IOL-811-205-K03x and BNI IOL-812-205-K03x
LED 13 … 20 are available ony for BNI IOL-812-205-K03x
LED x state
Value |
Description |
|---|---|
0 |
LED level will display Color B defined by ISDU |
1 |
LED level will display Color A defined by ISDU |
ISDU
Name |
Index |
Subindex |
Access |
Length |
Data Type |
DataStorage |
Default |
|---|---|---|---|---|---|---|---|
Flexible mode LED 1 Color A |
0x02B7 (695) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00FF0000 |
Flexible mode LED 2 Color A |
0x02B8 (696) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00FF0000 |
Flexible mode LED 3 Color A |
0x02B9 (697) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00FF0000 |
Flexible mode LED 4 Color A |
0x02BA (698) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00FF0000 |
Flexible mode LED 5 Color A |
0x02BB (699) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00808080 |
Flexible mode LED 6 Color A |
0x02BC (700) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00808080 |
Flexible mode LED 7 Color A |
0x02BD (701) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00808080 |
Flexible mode LED 8 Color A |
0x02BE (702) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00808080 |
Flexible mode LED 9 Color A |
0x02BF (703) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x0000FF00 |
Flexible mode LED 10 Color A |
0x02C0 (704) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x0000FF00 |
Flexible mode LED 11 Color A |
0x02C1 (705) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x0000FF00 |
Flexible mode LED 12 Color A |
0x02C2 (706) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x0000FF00 |
Flexible mode LED 13 Color A |
0x02C3 (707) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00FFFF00 |
Flexible mode LED 14 Color A |
0x02C4 (708) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00FFFF00 |
Flexible mode LED 15 Color A |
0x02C5 (709) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00FFFF00 |
Flexible mode LED 16 Color A |
0x02C6 (710) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00FFFF00 |
Flexible mode LED 17 Color A |
0x02C7 (711) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x000000FF |
Flexible mode LED 18 Color A |
0x02C8 (712) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x000000FF |
Flexible mode LED 19 Color A |
0x02C9 (713) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x000000FF |
Flexible mode LED 20 Color A |
0x02CA (714) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x000000FF |
Flexible mode LED 1 Color B |
0x02CB (715) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 2 Color B |
0x02CC (716) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 3 Color B |
0x02CD (717) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 4 Color B |
0x02CE (718) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 5 Color B |
0x02CF (719) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 6 Color B |
0x02D0 (720) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 7 Color B |
0x02D1 (721) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 8 Color B |
0x02D2 (722) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 9 Color B |
0x02D3 (723) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 10 Color B |
0x02D4 (724) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 11 Color B |
0x02D5 (725) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 12 Color B |
0x02D6 (726) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 13 Color B |
0x02D7 (727) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 14 Color B |
0x02D8 (728) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 15 Color B |
0x02D9 (729) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 16 Color B |
0x02DA (730) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 17 Color B |
0x02DB (731) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 18 Color B |
0x02DC (732) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 19 Color B |
0x02DD (733) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED 20 Color B |
0x02DE (734) |
0 |
R/W |
4 bytes |
UINT8 |
Yes |
0x00000000 |
Flexible mode LED X color Y
Bits |
Meaning |
|---|---|
0…7 |
8 bit value for component blue |
8…15 |
8 bit value for component green |
16…23 |
8 bit value for component red |
23…31 |
Reserved |
System Commands
Command Value |
Device Action |
|---|---|
0x81 (129) |
Application Reset – Reset ISDUs of Flexible mode indicator functionality to the default value. |
0x82 (130) |
Restore Factory Settings – Reset ISDUs of Flexible mode indicator functionality to the default value. |
For an overview of all System Commands, see section System Commands.