Segment mode

Description

The following chapters are relevant, in case the Segment mode mode has been selected via the SmartLight control feature.

General description: Segment indicator

Output Process Data

Note

Only mode dependent bytes are described in these chapter.

Byte

Description

Byte 0

Defined by other primary device functions

Byte 1

SmartLight control 2 and main signal function control
containing bitfield
Number of segments

Byte 2…3

Defined by other primary device functions

Byte 4

Segment 1 animation

Byte 5

Segment 1 color

Byte 6

Segment 2 animation

Byte 7

Segment 2 color

Byte 8

Segment 3 animation

Byte 9

Segment 3 color

Byte 10

Segment 4 animation

Byte 11

Segment 4 color

Byte 12

Segment 5 animation [1]

Byte 13

Segment 5 color [1]

Byte 14

Segment 6 animation [1]

Byte 15

Segment 6 color [1]

Byte 16…xx

Not used in this mode

Output process data bitfield descriptions

Number of segments

The number of the segments can be set. The auto scale functionality will set the number of segments automatically. Only segments, which have meaningful color setting, will be displayed, so that there will be no blank LEDs for inactive segments.

Value

Description

0

Reserved

1…6

Number of segements to be displayed [2]

7

Auto scale mode

Segment X animation

Bit

Description

Bit 0…3

Animation pattern

Bit 4

Animation direction

Bit 5

Reserved

Bit 6…7

Animation speed

Animation pattern

Value

Description

0x0

No animation, color A will be displayed

0x1

50% Blinking

0x2

Dynamic blink

0x3

Single strobe

0x4

Double strobe

0x5

Tripple strobe

0x6

Revolving

0x7

Rotating beacon

0x8

Custom blink 1

0x9

Custom blink 2

0xA

Custom blink 3

0xB…0xF

Reserved

Animation direction

The direction is relevant for the revolving segment animation pattern.

Value

Description

0

Top -> down

1

Bottom -> up

Animation speed

The animation speed values has different meaning depending on the selected animation pattern.

Value

Blink
Dynamic blink

Single strobe

Double strobe
Tripple storbe

Rotating beacon

Revolving

0

1 Hz

1 Hz

2/3 Hz

1 rev/sec

0.5 rev/sec

1

2 Hz

2 Hz

1 Hz

1.5 rev/sec

1 rev/sec

2

5 Hz

5 Hz

1.5 Hz

2 rev/sec

1.5 rev/sec

3

custom [3]

10 Hz

2 Hz

5 rev/sec

2 rev/sec

Segment X color

Bit

Value

Bit 0…3

Color A

Bit 4…7

Color B

Color A, Color B

Color A is the primary color. Without any animation the color A will be displayed. In case of an animation pattern has been set, the color of the segment will be changed between A and B according to the animation pattern.

Value

Description

0x0

Off

0x1

Red

0x2

Green

0x3

Yellow

0x4

Blue

0x5

Magenta

0x6

Cyan

0x7

White

0x8

Amber

0x9

User color 1

0xA

User color 2

0xB

User color 3

0xC

User color 4

0xD

User color 5

0xE

User color 6

0xF

User color 7

ISDU

Name

Index

Subindex

Access

Length

Data Type

DataStorage

Default

Custom Frequency of 50% blink

0x01C3 (451)

0

R/W

1 byte

UINT8

Yes

19

Custom Blink Pattern 1

0x01C4 (452)

0

R/W

32 bytes

UIN32

Yes

0x850A8000

Custom Blink Pattern 2

0x01C5 (453)

0

R/W

32 bytes

UIN32

Yes

0xA8508000

Custom Blink Pattern 3

0x01C6 (454)

0

R/W

32 bytes

UIN32

Yes

0xAA800000

Number of Samples in Custom Blink Pattern 1

0x01C7 (455)

0

R/W

1 byte

UINT8

Yes

28

Number of Samples in Custom Blink Pattern 2

0x01C8 (456)

0

R/W

1 byte

UINT8

Yes

28

Number of Samples in Custom Blink Pattern 3

0x01C9 (457)

0

R/W

1 byte

UINT8

Yes

20

Duration of Custom Blink Samples

0x01CA (458)

0

R/W

1 byte

UINT8 (ENUM)

Yes

5

Size of Revolving Segment

0x01CB (459)

0

R/W

1 byte

UINT8 (ENUM)

Yes

1

6 Segment Mode - Segment 1

0x01D1 (465)

0

R/W

2 bytes

UINT16

Yes

6 Segment Mode - Segment 2

0x01D2 (466)

0

R/W

2 bytes

UINT16

Yes

6 Segment Mode - Segment 3

0x01D3 (467)

0

R/W

2 bytes

UINT16

Yes

6 Segment Mode - Segment 4

0x01D4 (468)

0

R/W

2 bytes

UINT16

Yes

6 Segment Mode - Segment 5

0x01D5 (469)

0

R/W

2 bytes

UINT16

Yes

6 Segment Mode - Segment 6

0x01D6 (470)

0

R/W

2 bytes

UINT16

Yes

5 Segment Mode - Segment 1

0x01D7 (471)

0

R/W

2 bytes

UINT16

Yes

5 Segment Mode - Segment 2

0x01D8 (472)

0

R/W

2 bytes

UINT16

Yes

5 Segment Mode - Segment 3

0x01D9 (473)

0

R/W

2 bytes

UINT16

Yes

5 Segment Mode - Segment 4

0x01DA (474)

0

R/W

2 bytes

UINT16

Yes

5 Segment Mode - Segment 5

0x01DB (475)

0

R/W

2 bytes

UINT16

Yes

4 Segment Mode - Segment 1

0x01DC (476)

0

R/W

2 bytes

UINT16

Yes

4 Segment Mode - Segment 2

0x01DD (477)

0

R/W

2 bytes

UINT16

Yes

4 Segment Mode - Segment 3

0x01DE (478)

0

R/W

2 bytes

UINT16

Yes

4 Segment Mode - Segment 4

0x01DF (479)

0

R/W

2 bytes

UINT16

Yes

3 Segment Mode - Segment 1

0x01E0 (480)

0

R/W

2 bytes

UINT16

Yes

3 Segment Mode - Segment 2

0x01E1 (481)

0

R/W

2 bytes

UINT16

Yes

3 Segment Mode - Segment 3

0x01E2 (482)

0

R/W

2 bytes

UINT16

Yes

2 Segment Mode - Segment 1

0x01E3 (483)

0

R/W

2 bytes

UINT16

Yes

2 Segment Mode - Segment 2

0x01E4 (484)

0

R/W

2 bytes

UINT16

Yes

1 Segment Mode - Segment 1

0x01E5 (485)

0

R/W

2 bytes

UINT16

Yes

The customizable frequency of the 50% blinking can be set between 0.5 and 10 Hz in a step of 0.5 Hz.

Value

Frequency

0

0.5 Hz

1

1.0 Hz

2

1.5 Hz

3

2.0 Hz

4

2.5 Hz

5

3.0 Hz

6

3.5 Hz

7

4.0 Hz

8

4.5 Hz

9

5.0 Hz

10

5.5 Hz

11

6.0 Hz

12

6.5 Hz

13

7.0 Hz

14

7.5 Hz

15

8.0 Hz

16

8.5 Hz

17

9.0 Hz

18

9.5 Hz

19

10.0 Hz

The product provides three customizable animation patterns. Each pattern has a Custom Blink Pattern parameter that defines the actual animation sequence. For each pattern, the Number of Samples in Custom Blink Pattern register specifies how many samples (steps) the given pattern consists of. The Duration of Custom Blink Samples register defines the time duration of a single sample, and this duration is common for all three patterns. In other words, every sample within any custom blink pattern is displayed for the same, globally defined time.
The duration of a single periode of the aninmation pattern will be determined by the number of samples for the pattern, multiplied by the common sample duration.

Each bit of this parameter means a sample value for the blink pattern. Value 1 for the sample will result Color A to be signalized in the corresponding time slot, value 0 will display Color B. The bits will be displayed from direction MSB to LSB.

The number of the samples in the pattern can be set between 4 and 32.

Value

Sample time

0

50 ms

1

60 ms

2

70 ms

3

80 ms

4

90 ms

5

100 ms

6

120 ms

7

150 ms

8

200 ms

9

250 ms

10

500 ms

11

1000 ms

Size of Revolving Segment

The size of the revolving light can be configured. The exact amount of LED levels which are revolving will be automatic defined, becasue segment size may differ depending on other configurations.

Value

Description

0

Small

1

Medium

2

Large

X Segment Mode - Segment Y

The size of each segments can be configured independently. Different configurations are available depending on how many segments are selected as acitve segment. This description is relevan for all segments, in case of all possible number of segments selected. The ISDU adresses can be found at the ISDU table, here the subindex structure will be described. Each ISDU (for example 6 Segment Mode - Segment 5) has two numbers in their name. The first number (6 Segment mode) shows, that the ISDU is relevant, in case X (6 in the example) active segments has been set. The second number defines (Segment 5) which segment will be set. The ISDU value will define how big the segment shall be.
ISDU 6 Segment Mode - Segment 5 defines the size of the fifth segment, in case 6 segment mode has been selected.
The segment size can be defined by setting the lower and upper limit. The lower limit defines the first LED level, the upper limit defines the last LED level, which will be in the selected segment.

Note

The LEDs are equally splitted between the segments in case Number of segments has been set to auto scale mode, therefore X Segment Mode - Segment Y has no affect in such a case.

Name

Index

Subindex

Access

Length

Data Type

DataStorage

Default

X Segment Mode - Segment Y

0

R

2 bytes

yes

Lower

1

R

1 byte

UINT32

yes

–

Upper

2

R

1 byte

UINT32

yes

–

System Commands

Command Value

Device Action

0x81 (129)

Application Reset – Reset ISDUs of Segment indicator functionality to the default value.

0x82 (130)

Restore Factory Settings – Reset ISDUs of Segment indicator functionality to the default value.

For an overview of all System Commands, see section System Commands.