Voltage and Current Monitoring

Description

The voltage and current module sends messages about over-current, short-circuit, wire breakage, over-voltage and under-voltage. Over-voltage and under-voltage detection starts a timer. If the timer has expired and the voltage level has not returned to the normal operating voltage threshold, the module sends out the messages.

The messages include device status, IO-Link events, process data and LED signaling.

Mathematics/Algorithm

In SIO mode the threshold for undervoltage is 17V and for overvoltage is 32V.

If the device is in IO-Link mode, undervoltage occurs at 17V
and overvoltage occurs at 32V.

Process Data

Object ID

Name

Description

Direction

0x0017 (23)

Undervoltage

TRUE = the voltage level is below the threshold value.

Input

0x0018 (24)

Overvoltage

TRUE = the voltage level is above the threshold value.

Input

Also see section Process Data Profiles

ISDU

With the parameter Voltage Monitoring Detection Time Duration is possible to change the time between the detection of over/under voltage and the reporting of the event. (This parameter is used to eliminate unstable (transition) state as a filter)

Name

Index

Subindex

Access

Length

Data Type

Data Storage

Default

Voltage Monitoring Detection Time Duration

0x2200 (8704)

0

R/W

2 bytes

UINT16

Yes

10 (ms)

Voltage Monitoring Detection Time Duration

This parameter is used to define how long the under-voltage or over-voltage must be present before it is displayed. The unit is given in milliseconds. The values must be in the range between 10 and 1000. The default value is 10 milliseconds.

System Commands

Command Value

Device Action

0x81 (129)

Application Reset – Resets the Voltage Monitoring Detection Time Duration with ISDU-index 0x2200 to the default value 10.

0x82 (130)

Restore Factory Settings – Resets the Voltage Monitoring Detection Time Duration with ISDU-index 0x2200 to the default value 10.

For an overview of all System Commands, see section System Commands.

Events

Event Code

Event Type

Event – Description – Remedy

Device Status

0x5110

(20752)

Warning

Primary supply voltage exceeded
► Check for deviations in the supply.

2 – Out-of-Specification

0x5111

(20753)

Warning

Primary supply voltage below minimum value
► Check for deviations in the supply.

2 – Out-of-Specification

0x8D0B

(36107)

Warning

Overload or short circuit at pin 2
► Check wiring.

2 – Out-of-Specification

0x8D0D

(36109)

Warning

Incorrect load/cable breakage, analog current output pin 2
► Check wiring or connected devices.

2 – Out-of-Specification

0x8D15

(36117)

Warning

Overload at pin 2
► Check wiring.

2 – Out-of-Specification